3.2.1 Getting Started Application on PIC32CM GV VL Curiosity Nano+ Touch Evaluation Kit

Download

Description

This application illustrates how to control an LED using timer events and user interaction on the PIC32CM GV-Value Line Curiosity Nano+ Touch evaluation kit. The periodicity of the timeout will change from 500 milliseconds to 1 second, 2 seconds, 4 seconds and back to 500 milliseconds each time the switch on the PIC32CM GV-Value Line Curiosity Nano+ Touch evaluation kit is pressed.

When the LED toggling rate change, the current interval is printed to a serial terminal through UART, enabling users to observe the LED’s behavior directly on the board and monitor timing changes in real time through the terminal output.

Modules/Technology Used

  • Peripheral Modules
    • EIC
    • RTC
    • GPIO
    • SERCOM (USART)
    The following figure provides the MCC Harmony project graph with all the components.

Hardware Used

Software/Tools Used

This project has been verified to work with the following versions of software tools:

Refer to the Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/pic32cm_gv_vl_cnano.

  • Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
  • Any Serial Terminal application, such as Tera Term/PuTTY terminal application

Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).

Setup

  • Connect the PIC32CM GV-Value Line Curiosity Nano+ Touch evaluation kit to the host PC as a USB device through a Type-A male to Type-C® USB cable connected to Type-C USB (Debug USB) port

Programming Hex File

The pre-built hex file can be programmed by following the below steps.

Steps to program the hex file
  • Open MPLAB X IDE
  • Close all existing projects in IDE, if any project is opened.
  • Go to File>Import>Hex/ELF File
  • In the Import Image File window,
    1. Create Prebuilt Project,
      • Click the Browse button to select the prebuilt hex file
      • Select Device as PIC32CM3204GV00064.
      • Ensure the proper tool is selected under Hardware Tool and click the Next button
    2. Select Project Name and Folder,
      • Select appropriate project name and folder and click the Finish button
  • In MPLAB X IDE, click the Make and Program Device button to program the device
  • Follow the steps in Running the Demo section

Programming/Debugging Application Project

  • Open the project (pic32cm_gv_vl_cnano_getting_started/firmware/pic32cm_gv_vl_cnano.X) in MPLAB X IDE
  • Ensure PIC32CM GV VL Curiosity Nano is selected as hardware tool to program/debug the application
  • Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
  • Follow the steps in Running the Demo section

Running the Demo

  • Open the Tera Term/PuTTY terminal application on the PC (from the Windows® Start menu by pressing the Start button)
  • Set the baud rate to 115200
  • An LED on the PIC32CM GV-Value Line Curiosity Nano+ Touch evaluation kit toggles on every timeout basis
  • The default periodicity of the timeout is 500 milliseconds.
  • Press the switch on the PIC32CM GV-Value Line Curiosity Nano+ Touch evaluation kit to change the default periodicity of the timeout to 1 second
  • Every subsequent pressing of the switch SW200 on the PIC32CM GV-Value Line Curiosity Nano+ Touch evaluation kit changes the periodicity of the timeout to 2 seconds, 4 seconds, 500 milliseconds, and back to 1 second in cyclic order
  • The LED toggling rate is displayed on the serial terminal

Comments