9.18.1.1 +WAPC
This command is used to read or set the DCE’s hotspot access point configuration. This command is a configuration command which supports setting and getting parameter values. The behaviour of configuration commands is described in general in the 9.2.3 Configuration Commands section.
Security – Default Security for the command is: GGGG
|
Command |
Description |
Security |
|---|---|---|
|
|
Query all configuration elements |
|
|
|
Query a single element |
|
|
|
Set a single element |
|
|
Parameter Name |
Type |
Description |
|---|---|---|
|
|
Integer |
Parameter ID number |
|
|
Integer String Byte Array |
Parameter value |
|
Response |
Description |
|---|---|
|
|
Read response |
|
Element Name |
Type |
Description |
|---|---|---|
|
|
Integer |
Parameter ID number |
|
|
Any |
Parameter value |
|
ID |
Name |
Type |
Description |
Security |
|---|---|---|---|---|
|
1 |
|
String |
Network Name Maximum length is 32 |
|
|
2 |
|
Integer |
Security Type
|
|
|
3 |
|
String |
Credentials required for connecting to the network of the security type specified Maximum length is 128 |
|
|
4 |
|
Integer |
The channel on which to set up the network. Valid range is 1-13 |
|
|
5 |
|
Bool |
Visibility of the network
|
|
|
7 |
|
Bool |
Layer 2 only flag
|
|
|
8 |
|
Unsigned Integer |
Network interface index |
|