9.19.1.1 +WSCNC
This command is used to modify or query the behavior of the active scanning function. This command is a configuration command which supports setting and getting parameter values. The behaviour of configuration commands is described in general in the 9.2.3 Configuration Commands section.
Security – Default Security for the command is: GGGG
|
Command |
Description |
Security |
|---|---|---|
|
|
Query all configuration elements |
|
|
|
Query a single element |
|
|
|
Set a single element |
|
|
Parameter Name |
Type |
Description |
|---|---|---|
|
|
Integer |
Parameter ID number |
|
|
Integer String Byte Array |
Parameter value |
|
Response |
Description |
|---|---|
|
|
Read response |
|
Element Name |
Type |
Description |
|---|---|---|
|
|
Integer |
Parameter ID number |
|
|
Any |
Parameter value |
|
ID |
Name |
Type |
Description |
Security |
|---|---|---|---|---|
|
1 |
|
Unsigned Integer |
Channel to scan (or 0 for all channels) |
|
|
2 |
|
Unsigned Integer |
The time in milliseconds to wait for probe responses |
|
|
3 |
|
Unsigned Integer |
The time in milliseconds to wait for beacons |
|
|
4 |
|
Unsigned Integer |
Number of scan slots |
|
|
5 |
|
Unsigned Integer |
Number of probes sent per active slot |
|
|
6 |
|
Integer |
RSSI threshold (or 0 for none) |
|
|
7 |
|
Unsigned Integer |
Security filter, bitmask of:
|
|
|
8 |
|
Bool |
Asynchronous notification
|
|
|
10 |
|
Byte Array |
SSID filter list This is a multiple value parameter with the range 10.0-10.3 |
|
|
20 |
|
Complex Value1 (Read Only) |
Top scan results from previous scan, ordered by RSSI This is a multiple value parameter with the range 20.0-20.7 |
|
|
No. |
Complex Value |
Description |
|---|---|---|
|
1 |
|
Scan indicator |
|
Element Name |
Type |
Description |
|---|---|---|
|
|
Integer |
Received signal strength |
|
|
Integer |
Recommended security type to use when connecting to this AP
|
|
|
Integer |
The channel number of the detected device |
|
|
String |
The BSSID of detected device |
|
|
String |
SSID of detected device |