2 ADC Example Component, Running the Examples
2.1 Running the ADC Basic Printf Example
When using the MPLAB Data Visualizer Time Plot to run the ADC Basic Printf example, the following will appear:
See related GitHub examples:
The following video shows a similar example from the MCC Melody API Reference for PIC16F/18F MCU Families.
2.2 Running the ADC Data Streamer Example
When using the MPLAB Data Visualizer Time Plot to run the ADC Basic Printf example, the following will appear:
See related GitHub example: github.com/microchip-pic-avr-examples/pic18f57q43-adcc-data-streamer-callbacks-mcc
The following video shows a similar example from the MCC Melody API Reference for PIC16F/18F MCU Families.
2.3 Running the ADCC Spike Detection Example
adcResult_lastSpike and adcSpikeCount
variables.
The following video shows a similar example from the MCC Melody API Reference for PIC16F/18F MCU Families.
2.4 Example Board for the ADCC Examples
The ADCC example can be run on Curiosity Nano boards, such as the PIC18F-Q41 or PIC18F-Q43. The image below shows an ADC reading of the Q43, taken by using the potentiometer on the Curiosity Nano Explorer.
All three ADCC examples were tested using the hardware setup presented below.