2.4 RMS Voltage Measurement
For the A/C power supply, RMS is equal to the value of the direct current that would produce the same average power dissipation in a resistive load. The RMS value gives the equivalent DC measurement of the A/C power. Mathematically, the root mean square is defined as the square root of the mean square (the arithmetic mean of the squares of a set of numbers). In alternating signals, RMS can be defined as an integral of the squares of the instantaneous values during a cycle.
In the application, the RMS voltage is calculated by the arithmetic mean of the square of a set of numbers on a phase of the three-phase input signal.
Equation for calculating RMS voltage:
Here,
- N is the total number of samples
- n is the sample number and the possible values are 1, 2, 3, 4...n
- V1, V2, V3...Vn represent the voltage (in mV) of the sampled data points
- ADCCOUTn is the equivalent digital output value for each sampled input signal
- ADCC Step Size is,
Here the ADCC is provided by a reference voltage (Vref) of 3.3V. It provides a 10-bit binary result using successive approximation, which gives the Resolution (R) of ADCC equal to 10.
Therefore, value of ADCC step size is,