2.2.3.1 DIAG_EEPROM_CalculateStoreCRC()
diag_result_t DIAG_EEPROM_CalculateStoreCRC (eeprom_address_t startAddress, uint16_t length, eeprom_address_t storeAddress)
Calculates 32-bit CRC for a given EEPROM memory region and stores it at the EEPROM address indicated by the storeAddress argument.
| in | startAddress |
- Starting address of EEPROM memory region to be considered for CRC |
| in | length |
- Number of bytes from startAddress to be considered for CRC |
| in | storeAddress |
- The EEPROM address where calculated CRC will be stored |
DIAG_PASS - CRC for given EEPROM region is calculated and stored successfully DIAG_INVALID_ARG - An invalid argument is passed to the function DIAG_NVM_STORE_ERROR - An error occurred while storing the calculated CRC in EEPROM Calculates 32-bit CRC for a given EEPROM memory region and stores it at the EEPROM address indicated by the storeAddress argument. |
| in | startAddress |
Starting address of the EEPROM memory region to be considered for CRC |
| in | length |
Number of bytes from startAddress to be considered for CRC |
| in | storeAddress |
The EEPROM address where calculated CRC will be stored |
DIAG_PASS - CRC for given EEPROM region is calculated and stored successfully DIAG_INVALID_ARG - An invalid argument is passed to the function DIAG_NVM_STORE_ERROR - An error occurred while storing the calculated CRC in EEPROM |