8.2 Random Read
A random read begins in the same way as a byte write operation does
to load in a new data word address. This is known as a “dummy write” sequence; however, the
data byte and the Stop condition of the byte write must be omitted to prevent the part from
entering an internal write cycle. Once the device address and word address are clocked in
and acknowledged by the EEPROM, the bus host must generate another Start condition. The bus
host now initiates a current address read by sending a Start condition, followed by a valid
device address byte with the R/W bit set to
logic ‘1
’. The EEPROM will ACK the device address and serially clock
out the data word on the SDA line. All types of read operations will be terminated if the
bus host does not respond with an ACK (it NACKs) during the ninth clock cycle. After the
NACK response, the host may send a Stop condition to complete the protocol, or it can send
a Start condition to begin the next sequence.