4.2.4 QTouch Button
There is one self capacitance button available on the SAM L21 Xplained Pro board that can be used as I/O. This QTouch button is intended to be driven by the built-in Peripheral Touch Controller (PTC) of the device. A zero ohm resistor is added on the board to easily disconnect the onboard touch buttons from the extension header, as the I/O lines are shared between the two.
| SAM L21 pin | Silkscreen text | Shared functionality |
|---|---|---|
| PA10 | QT BTN1 | EXT2 |