4.2.2 Mechanical Buttons
SAM L21 Xplained Pro contains two mechanical buttons. One button is the RESET button connected to the SAM L21 reset line and the other is a generic user configurable button. When a button is pressed it will drive the I/O line to GND.
Note: There is no pull-up resistor connected to the
generic user button. Remember to enable the internal pull-up in the SAM
L21 to use the button.
| SAM L21 pin | Silkscreen text | Shared functionality |
|---|---|---|
| RESET | RESET | - |
| PA02 | SW0 | EXT1 |