ULP0 Mode Operation
ULP0 mode maintains very low frequency clocks (MCK1, CPU_CLK) in the system to wake up on any interrupt. Selection of the clock frequency depends on the current consumption target versus the required wake-up time. The higher the frequency, the higher the power consumption and the faster the wake-up time.
The sequence to enter ULP0 mode is detailed below. The code used to enter this mode must be executed out of the internal SRAM. Steps 1 to 6 are meant to bypass the DDR delay lines so as to avoid their power consumption.
Entering ULP0 Mode
- Enter SDRAM Self-refresh mode (if used).
- Turn on DDR PLL (if DDR was not used).
- Reset the DDR Controller using RSTC_GRSTR.
- Wait until the status bit is asserted.
- Program the lane and control delay lines bypass using the DDLDIS bit in DDR3PHY_ACDLLCR, DDR3PHY_DX0DLLCR and DDR3PHY_DX1DLLCR registers.
- Turn off DDRPLL in PMC.
- Set the interrupts to wake up the system.
- Disable all peripheral clocks.
- Set the I/Os to an appropriate state and suspend the USB transceivers.
- Switch the system clock to MD_SLCK.
- Disable the PLLs, the Main Crystal Oscillator and the Main RC Oscillator.
- Enter the Wait for Interrupt (WFI) mode.
Exiting ULP0 Mode
Wake-up from ULP0 mode is triggered by any enabled interrupt. When resuming, the software reconfigures the system (oscillator, PLL, etc.) to the same state as before WFI.