11.1.6 I/O Characteristics
The device features the following types of input/output (I/O) circuits:
- GPIO I/Os with drive and slewrate
control.
- AUDIOCLK is a special case of GPIO type with hardwired DRIVE and SR
controls.
- For AUDIOCLK: DRIVE = 0 and SR = 1
- AUDIOCLK is a special case of GPIO type with hardwired DRIVE and SR
controls.
- HSIO I/Os with drive control only for
the following lines:
- SDMMC0: PA0, PA1, PA3, PA4, PA5, PA6, PA7, PA8, PA9, PA10, PA11
- SDMMC1: PB29, PB30, PB31, PC0, PC1, PC2
- SDMMC2: PD3, PD4, PD5, PD6, PD7, PD8
- QSPI0: PB9, PB10, PB11, PB12, PB14, PB15, PB16, PB17, PB18, PB19, PB20
- PIOBU I/Os with no drive and no slewrate control
Unless otherwise specified:
- The following specifications apply to the GPIO, PIOBU and HSIO types.
- VDD refers to the voltage of the associated power rail of the I/O line, as defined in the Pin Description table; for example, for PA12, VDD refers to the voltage applied on VDDIOP0.
For SDMMC lines in UHS I mode in the 1.8V range, the drive is controlled in the SDMMC user interface. In this case, drive configurations in PIO registers have no effect.
For any other SDMMC configuration, the GPIO drive configuration is applicable.
DRIVE and SLEWRATE are set in the PIO_CFGR register corresponding to the GPIO, with the DRVSTR and SR bits, respectively.