1.8.2.3 Pin Description

The device features several PIO controllers that multiplex the I/O lines of the peripheral set. The following Pin Description table defines how the I/O lines are multiplexed on the different PIO controllers. The "Reset State" column shows whether the PIO line resets in I/O mode or in Peripheral mode. If I/O is shown, the PIO line resets with the characteristics (input, output, pull–up or pull–down) indicated in this same column, so that the device is configured in a known state as soon as the reset is released. As a result, PIO_CFGR.FUNC resets to ‘0’. If a signal name is shown in the “Reset State” column, the PIO line is assigned to this function and PIO_CFGR.FUNC is not set to ‘0’. That is the case for pins controlling memories, in particular address lines, which require the pin to be driven as soon as the reset is released.

Table 1-3. Pin Description(1)(2)

343–pin
TFBGA

375–pin
TFBGA

Power
Rail

I/O
Type(3)

PrimaryAlternatePIO PeripheralReset State(4)
     Signal     DirSignalDirFuncSignalDirI/O Set

Signal, Dir, PU,
PD, HiZ, ST

H17P19VDDSDMMC0HSIOPA0I/O––ASDMMC0_CKO1PIO, I, PU, ST
BFLEXCOM0_IO0I/O1
CCANTX3O1
EPWML0O3
G20T21VDDSDMMC0HSIOPA1I/O––ASDMMC0_CMDI/O1PIO, I, PU, ST
BFLEXCOM0_IO1I/O1
CCANRX3I1
DD14I/O1,2
EPWMH0O3
L13P20VDDSDMMC0GPIOPA2I/O––ASDMMC0_RSTNO1PIO, I, PU, ST
BFLEXCOM0_IO2I/O1
CPDMC1_CLKO1
DD15I/O1,2
EPWMH1O3
FFLEXCOM1_IO0I/O3
L14R21VDDSDMMC0HSIOPA3I/O––ASDMMC0_DAT0I/O1PIO, I, PU, ST
BFLEXCOM0_IO3I/O1
CPDMC1_DS0I1
DNWR1/NBS1O1,2
EPWML3O3
FFLEXCOM1_IO1I/O3
K13N18VDDSDMMC0HSIOPA4I/O––ASDMMC0_DAT1I/O1PIO, I, PU, ST
BFLEXCOM0_IO4O1
CPDMC1_DS1I1
DNCS2O1,2
EPWMH3O3
FFLEXCOM2_IO0I/O3
C21P21VDDSDMMC0HSIOPA5I/O––ASDMMC0_DAT2I/O1PIO, I, PU, ST
BFLEXCOM1_IO0I/O1
CCANTX2O1
DA23O1,2
EPWMEXTRG0I3
FFLEXCOM2_IO1I/O3
K14R18VDDSDMMC0HSIOPA6I/O––ASDMMC0_DAT3I/O1PIO, I, PU, ST
BFLEXCOM1_IO1I/O1
CCANRX2I1
DA24O1,2
EPWMEXTRG1I3
FFLEXCOM3_IO0I/O3
H16P18VDDSDMMC0HSIOPA7I/O––ASDMMC0_DAT4I/O1PIO, I, PU, ST
BFLEXCOM2_IO0I/O1
CCANTX1O1
DNWAITI1,2
EPWMFI0I3
FFLEXCOM3_IO1I/O3
B21N20VDDSDMMC0HSIOPA8I/O––ASDMMC0_DAT5I/O1PIO, I, PU, ST
BFLEXCOM2_IO1I/O1
CCANRX1I1
DNCS0O1,2
EPWMFI1I3
FFLEXCOM4_IO0I/O3
D20M20VDDSDMMC0HSIOPA9I/O––ASDMMC0_DAT6I/O1PIO, I, PU, ST
BFLEXCOM2_IO2I/O1
CCANTX0O1
DSMCKO1,2
ESPDIF_RXI1
FFLEXCOM4_IO1I/O3
J15L18VDDSDMMC0HSIOPA10I/O––ASDMMC0_DAT7I/O1PIO, I, PU, ST
BFLEXCOM2_IO3I/O1
CCANRX0I1
DNCS1O1,2
ESPDIF_TXO1
FFLEXCOM5_IO0I/O3
F20M19VDDSDMMC0HSIOPA11I/O––ASDMMC0_DSI1PIO, I, PU, ST
BFLEXCOM2_IO4O1
DA0/NBS0O1,2
ETIOA0I/O1
FFLEXCOM5_IO1I/O3
V14V7VDDIOP0GPIOPA12I/O––ASDMMC0_WPI1PIO, I, PU, ST
BFLEXCOM1_IO3I/O1
DFLEXCOM3_IO5O1
EPWML2O3
FFLEXCOM6_IO0I/O3
AA16Y9VDDIOP0GPIOPA13I/O––ASDMMC0_1V8SELO1PIO, I, PU, ST
BFLEXCOM1_IO2I/O1
DFLEXCOM3_IO6O1
EPWMH2O3
FFLEXCOM6_IO1I/O3
AA20AA10VDDIOP0GPIOPA14I/O––ASDMMC0_CDI1PIO, I, PU, ST
BFLEXCOM1_IO4O1
DA25O1,2
EPWML1O3
V15V9VDDIOP0GPIOPA15I/O––AG0_TXEN/G0_TXCTLO1PIO, I, PU, ST
BFLEXCOM3_IO0I/O1
CISC_MCKO1
DA1O1,2
ETIOB0I/O1
Y15AA11VDDIOP0GPIOPA16I/O––AG0_TX0O1PIO, I, PU, ST
BFLEXCOM3_IO1I/O1
CISC_D0I1
DA2O1,2
ETCLK0I1
V16Y10VDDIOP0GPIOPA17I/O––AG0_TX1O1PIO, I, PU, ST
BFLEXCOM3_IO2I/O1
CISC_D1I1
DA3O1,2
ETIOA1I/O1
Y16Y11VDDIOP0GPIOPA18I/O––AG0_RXDV/G0_CRSDV/G0_RXCTLI1PIO, I, PU, ST
BFLEXCOM3_IO3I/O1
CISC_D2I1
DA4O1,2
ETIOB1I/O1
V20V10VDDIOP0GPIOPA19I/O––AG0_RX0I1PIO, I, PU, ST
BFLEXCOM3_IO4O1
CISC_D3I1
DA5O1,2
ETCLK1I1
Y21V12VDDIOP0GPIOPA20I/O––AG0_RX1I1PIO, I, PU, ST
BFLEXCOM4_IO0I/O1
CISC_D4I1
DA6O1,2
ETIOA2I/O1
V21V8VDDIOP0GPIOPA21I/O––AG0_RXERI1PIO, I, PU, ST
BFLEXCOM4_IO1I/O1
CISC_D5I1
DA7O1,2
ETIOB2I/O1
Y18Y12VDDIOP0GPIOPA22I/O––AG0_MDCO1PIO, I, PU, ST
BFLEXCOM4_IO2I/O1
CISC_D6I1
DA8O1,2
ETCLK2I1
R13V11VDDIOP0GPIOPA23I/O––AG0_MDIOI/O1PIO, I, PU, ST
BFLEXCOM4_IO3I/O1
CISC_D7I1
DA9O1,2
Y19W12VDDIOP0GPIOPA24I/O––AG0_TXCK/G0_REFCKI/O1PIO, I, PU, ST
BFLEXCOM4_IO4O1
CISC_HSYNCI1
DA10O1,2
EFLEXCOM0_IO5O1
U14AA12VDDIOP0GPIOPA25I/O––AG0_125CKI1PIO, I, PU, ST
BFLEXCOM5_IO4O1
CISC_VSYNCI1
DA11O1,2
EFLEXCOM0_IO6O1
FFLEXCOM7_IO0I/O3
W16V13VDDIOP0GPIOPA26I/O––AG0_TX2O1PIO, I, PU, ST
BFLEXCOM5_IO2I/O1
CISC_FIELDI1
DA12O1,2
ETF0I/O1
FFLEXCOM7_IO1I/O3
W18Y13VDDIOP0GPIOPA27I/O––AG0_TX3O1PIO, I, PU, ST
BFLEXCOM5_IO3I/O1
CISC_PCKI1
DA13O1,2
ETK0I/O1
FFLEXCOM8_IO0I/O3
T14W13VDDIOP0GPIOPA28I/O––AG0_RX2I1PIO, I, PU, ST
BFLEXCOM5_IO0I/O1
CISC_D8I1
DA14O1,2
ERD0I1
FFLEXCOM8_IO1I/O3
W19AA14VDDIOP0GPIOPA29I/O––AG0_RX3I1PIO, I, PU, ST
BFLEXCOM5_IO1I/O1
CISC_D9I1
DA15O1,2
ERF0I/O1
FFLEXCOM9_IO0I/O3
R14V14VDDIOP0GPIOPA30I/O––AG0_RXCKI1PIO, I, PU, ST
BFLEXCOM6_IO4O1
CISC_D10I1
DA16O1,2
ERK0I/O1
FFLEXCOM9_IO1I/O3
W20Y14VDDIOP0GPIOPA31I/O––AG0_TXERO1PIO, I, PU, ST
BFLEXCOM6_IO2I/O1
CISC_D11I1
DA17O1,2
ETD0O1
FFLEXCOM10_IO0I/O3
U18W14VDDIOP0GPIOPB0I/O––AG0_COLI1PIO, I, PU, ST
BFLEXCOM6_IO3I/O1
CEXT_IRQ0I1
DA18O1,2
ESPDIF_RXI2
FFLEXCOM10_IO1I/O3
W21W15VDDIOP0GPIOPB1I/O––AG0_CRSI1PIO, I, PU, ST
BFLEXCOM6_IO1I/O1
CEXT_IRQ1I1
DA19O1,2
ESPDIF_TXO2
FFLEXCOM11_IO0I/O3
T21V15VDDIOP0GPIOPB2I/O––AG0_TSUCOMPO1PIO, I, PU, ST
BFLEXCOM6_IO0I/O1
CADTRGI1
DA20O1,2
FFLEXCOM11_IO1I/O3
V19Y15VDDIOP0GPIOPB3I/O––ARF1I/O1PIO, I, PU, ST
BFLEXCOM11_IO0I/O1
CPCK2O2
DD8I/O1,2
T20V17VDDIOP0GPIOPB4I/O––ATF1I/O1PIO, I, PU, ST
BFLEXCOM11_IO1I/O1
CPCK3O2
DD9I/O1,2
V18AA15VDDIOP0GPIOPB5I/O––ATK1I/O1PIO, I, PU, ST
BFLEXCOM11_IO2I/O1,2,3,4,5
CPCK4O2
DD10I/O1,2
T19V16VDDIOP0GPIOPB6I/O––ARK1I/O1PIO, I, PU, ST
BFLEXCOM11_IO3I/O1,2,3,4,5
CPCK5O2
DD11I/O1,2
V17Y16VDDIOP0GPIOPB7I/O––ATD1O1PIO, I, PU, ST
BFLEXCOM11_IO4O1,2,3,4,5
CFLEXCOM3_IO5O2,3,4,5
DD12I/O1,2
T18Y17VDDIOP0GPIOPB8I/O––ARD1I1PIO, I, PU, ST
BFLEXCOM8_IO0I/O1
CFLEXCOM3_IO6O2,3,4,5
DD13I/O1,2
P17AA20VDDQSPI0HSIOPB9I/O––AQSPI0_IO3I/O1PIO, I, PU, ST
BFLEXCOM8_IO1I/O1
CPDMC0_CLKO1
DNCS3/NANDCSO1
EPWML0O2
P15W18VDDQSPI0HSIOPB10I/O––AQSPI0_IO2I/O1PIO, I, PU, ST
BFLEXCOM8_IO2I/O1
CPDMC0_DS0I1
DNWE/NWR0/NANDWEO1
EPWMH0O2
G21U19VDDQSPI0HSIOPB11I/O––AQSPI0_IO1I/O1PIO, I, PU, ST
BFLEXCOM8_IO3I/O1
CPDMC0_DS1I1
DNRD/NANDOEO1
EPWML1O2
M15T18VDDQSPI0HSIOPB12I/O––AQSPI0_IO0I/O1PIO, I, PU, ST
BFLEXCOM8_IO4O1
CFLEXCOM6_IO5O1
DA21/NANDALEO1
EPWMH1O2
R16W17VDDQSPI0GPIOPB13I/O––AQSPI0_CSO1PIO, I, PU, ST
BFLEXCOM9_IO0I/O1
CFLEXCOM6_IO6O1
DA22/NANDCLEO1
EPWML2O2
N14W21VDDQSPI0HSIOPB14I/O––AQSPI0_SCKO1PIO, I, PU, ST
BFLEXCOM9_IO1I/O1
DD0I/O1
EPWMH2O2
N15Y21VDDQSPI0HSIOPB15I/O––AQSPI0_SCKNO1PIO, I, PU, ST
BFLEXCOM9_IO2I/O1
DD1I/O1
EPWML3O2
M14R20VDDQSPI0HSIOPB16I/O––AQSPI0_IO4I/O1PIO, I, PU, ST
BFLEXCOM9_IO3I/O1
CPCK0O1
DD2I/O1
EPWMH3O2
FEXT_IRQ0I2
F21U20VDDQSPI0HSIOPB17I/O––AQSPI0_IO5I/O1PIO, I, PU, ST
BFLEXCOM9_IO4O1
CPCK1O1
DD3I/O1
EPWMEXTRG0I2
FEXT_IRQ1I2
D21T20VDDQSPI0HSIOPB18I/O––AQSPI0_IO6I/O1PIO, I, PU, ST
BFLEXCOM10_IO0I/O1
CPCK2O1
DD4I/O1
EPWMEXTRG1I2
M13R19VDDQSPI0HSIOPB19I/O––AQSPI0_IO7I/O1PIO, I, PU, ST
BFLEXCOM10_IO1I/O1
CPCK3O1
DD5I/O1
EPWMFI0I2
J21V19VDDQSPI0HSIOPB20I/O––AQSPI0_DQSI1PIO, I, PU, ST
BFLEXCOM10_IO2I/O1,2,3,4,5
DD6I/O1
EPWMFI1I2
J20U21VDDQSPI0GPIOPB21I/O––AQSPI0_INTI1PIO, I, PU, ST
BFLEXCOM10_IO3I/O1,2,3,4,5
CFLEXCOM9_IO5O1
DD7I/O1
H15K18VDDQSPI1GPIOPB22I/O––AQSPI1_IO3I/O1PIO, I, PU, ST
BFLEXCOM10_IO4O1,2,3,4,5
CFLEXCOM9_IO6O1
DNANDRDYI1
F19L19VDDQSPI1GPIOPB23I/O––AQSPI1_IO2I/O1PIO, I, PU, ST
BFLEXCOM7_IO0I/O1
CI2SMCC0_CKI/O1
FPCK4O1
G19L21VDDQSPI1GPIOPB24I/O––AQSPI1_IO1I/O1PIO, I, PU, ST
BFLEXCOM7_IO1I/O1
CI2SMCC0_WSI/O1
FPCK5O1
J14M18VDDQSPI1GPIOPB25I/O––AQSPI1_IO0I/O1PIO, I, PU, ST
BFLEXCOM7_IO2I/O1
CI2SMCC0_DOUT1O1
FPCK6O1
C20L20VDDQSPI1GPIOPB26I/O––AQSPI1_CSO1PIO, I, PU, ST
BFLEXCOM7_IO3I/O1
CI2SMCC0_DOUT0O1
EPWMEXTRG0I1
FPCK7O1
G16J20VDDQSPI1GPIOPB27I/O––AQSPI1_SCKO1PIO, I, PU, ST
BFLEXCOM7_IO4O1
CI2SMCC0_MCKO1
EPWMEXTRG1I1
G10A18VDDSDMMC1GPIOPB28I/O––ASDMMC1_RSTNO1PIO, I, PU, ST
BADTRGI2
EPWMFI0I1
FFLEXCOM7_IO0I/O4
H11A20VDDSDMMC1HSIOPB29I/O––ASDMMC1_CMDI/O1PIO, I, PU, ST
BFLEXCOM3_IO2I/O2,3,4,5
CFLEXCOM0_IO5O2
DTIOA3I/O1
EPWMFI1I1
FFLEXCOM7_IO1I/O4
B9A16VDDSDMMC1HSIOPB30I/O––ASDMMC1_CKO1PIO, I, PU, ST
BFLEXCOM3_IO3I/O2,3,4,5
CFLEXCOM0_IO6O2
DTIOB3I/O1
EPWMH0O1
FFLEXCOM8_IO0I/O4
A13A19VDDSDMMC1HSIOPB31I/O––ASDMMC1_DAT0I/O1PIO, I, PU, ST
BFLEXCOM3_IO4O2,3,4,5
CFLEXCOM9_IO5O2,3,4,5
DTCLK3I1
EPWML0O1
FFLEXCOM8_IO1I/O4
A9B18VDDSDMMC1HSIOPC0I/O––ASDMMC1_DAT1I/O1PIO, I, PU, ST
BFLEXCOM3_IO0I/O2
DTIOA4I/O1
EPWML1O1
FFLEXCOM9_IO0I/O4
H10D12VDDSDMMC1HSIOPC1I/O––ASDMMC1_DAT2I/O1PIO, I, PU, ST
BFLEXCOM3_IO1I/O2
DTIOB4I/O1
EPWMH1O1
FFLEXCOM9_IO1I/O4
A7C13VDDSDMMC1HSIOPC2I/O––ASDMMC1_DAT3I/O1PIO, I, PU, ST
BFLEXCOM4_IO0I/O2
DTCLK4I1
EPWML2O1
FFLEXCOM10_IO0I/O4
G1B2VDDIN33GPIOPC3I/O––ASDMMC1_WPI1PIO, I, PU, ST
BFLEXCOM4_IO1I/O2
DTIOA5I/O1
EPWMH2O1
FFLEXCOM10_IO1I/O4
H5E4VDDIN33GPIOPC4I/O––ASDMMC1_CDI1PIO, I, PU, ST
BFLEXCOM4_IO2I/O2,3,4,5
CFLEXCOM9_IO6O2,3,4,5
DTIOB5I/O1
EPWML3O1
FFLEXCOM11_IO0I/O4
F2D4VDDIN33GPIOPC5I/O––ASDMMC1_1V8SELO1PIO, I, PU, ST
BFLEXCOM4_IO3I/O2,3,4,5
CFLEXCOM6_IO5O2,3,4,5
DTCLK5I1
EPWMH3O1
FFLEXCOM11_IO1I/O4
K8G4VDDIN33GPIOPC6I/OACC_INP0–BFLEXCOM4_IO4O2,3,4,5PIO, I, PU, ST
CFLEXCOM6_IO6O2,3,4,5
J8E3VDDIN33GPIOPC7I/OACC_INN1–AI2SMCC0_DIN0I1PIO, I, PU, ST
BFLEXCOM7_IO0I/O2
F1D3VDDIN33GPIOPC8I/OACC_INP1–AI2SMCC0_DIN1I1PIO, I, PU, ST
BFLEXCOM7_IO1I/O2
G2C4VDDIN33GPIOPC9I/OACC_INN2–AI2SMCC0_DOUT3O1PIO, I, PU, ST
BFLEXCOM7_IO2I/O2,3,4,5
FFLEXCOM1_IO0I/O4
M10H3VDDIN33GPIOPC10I/OACC_INP2–AI2SMCC0_DOUT2O1PIO, I, PU, ST
BFLEXCOM7_IO3I/O2,3,4,5
FFLEXCOM1_IO1I/O4
K9F4VDDIN33GPIOPC11I/OACC_INN3–AI2SMCC1_CKI/O1PIO, I, PU, ST
BFLEXCOM7_IO4O2,3,4,5
FFLEXCOM2_IO0I/O4
D1G3VDDIN33GPIOPC12I/OACC_INP3–AI2SMCC1_WSI/O1PIO, I, PU, ST
BFLEXCOM8_IO2I/O2,3,4,5
FFLEXCOM2_IO1I/O4
F8D10VDDIN33GPIOPC13I/OAD0–AI2SMCC1_MCKO1PIO, I, PU, ST
BFLEXCOM8_IO1I/O2
FFLEXCOM3_IO0I/O4
D6B7VDDIN33GPIOPC14I/OAD1–AI2SMCC1_DOUT0O1PIO, I, PU, ST
BFLEXCOM8_IO0I/O2
FFLEXCOM3_IO1I/O4
H9B9VDDIN33GPIOPC15I/OAD2–AI2SMCC1_DOUT1O1PIO, I, PU, ST
BFLEXCOM8_IO3I/O2,3,4,5
FFLEXCOM4_IO0I/O4
D5A7VDDIN33GPIOPC16I/OAD3–AI2SMCC1_DOUT2O1PIO, I, PU, ST
BFLEXCOM8_IO4O2,3,4,5
FFLEXCOM4_IO1I/O4
D3C6VDDIN33GPIOPC17I/OAD4/RTCOUT0–AI2SMCC1_DOUT3O1PIO, I, PU, ST
BEXT_IRQ0I3
FFLEXCOM5_IO0I/O4
C4B6VDDIN33GPIOPC18I/OAD5/RTCOUT1–AI2SMCC1_DIN0I1PIO, I, PU, ST
BFLEXCOM9_IO0I/O2
FFLEXCOM5_IO1I/O4
G8C9VDDIN33GPIOPC19I/OAD6–AI2SMCC1_DIN1I1PIO, I, PU, ST
BFLEXCOM9_IO1I/O2
FFLEXCOM6_IO0I/O4
D4B5VDDIN33GPIOPC20I/OAD7–AI2SMCC1_DIN2I1PIO, I, PU, ST
BFLEXCOM9_IO4O2,3,4,5
FFLEXCOM6_IO1I/O4
E4C10VDDIN33GPIOPC21I/OAD8–AI2SMCC1_DIN3I1PIO, I, PU, ST
BFLEXCOM9_IO2I/O2,3,4,5
DD3I/O2
FFLEXCOM6_IO0I/O5
C3C5VDDIN33GPIOPC22I/OAD9–AI2SMCC0_DIN2I1PIO, I, PU, ST
BFLEXCOM9_IO3I/O2,3,4,5
DD4I/O2
FFLEXCOM6_IO1I/O5
F3A4VDDIN33GPIOPC23I/OAD10–AI2SMCC0_DIN3I1PIO, I, PU, ST
BFLEXCOM0_IO5O3
DD5I/O2
FFLEXCOM7_IO0I/O5
C2D6VDDIN33GPIOPC24I/OAD11–BFLEXCOM0_IO6O3PIO, I, PU, ST
CEXT_IRQ1I3
DD6I/O2
FFLEXCOM7_IO1I/O5
B1B3VDDIN33GPIOPC25I/O––ANTRSTI1NTRST, PU, ST
H7D7VDDIN33GPIOPC26I/O––ATCK_SWCLKI1TCK_SWCLK, ST
C1B1VDDIN33GPIOPC27I/O––ATMS_SWDIOI/O1TMS_SWDIO, PU, ST
H6C2VDDIN33GPIOPC28I/O––ATDII1TDI, PU, ST
A2B4VDDIN33GPIOPC29I/O––ATDOO1TDO, ST
G4A6VDDIN33GPIOPC30I/OAD12–BFLEXCOM10_IO0I/O2PIO, I, PD, ST
D2D8VDDIN33GPIOPC31I/OAD13–BFLEXCOM10_IO1I/O2PIO, I, PD, ST
G3D5VDDIN33GPIOPD0I/OAD14–BFLEXCOM11_IO0I/O2PIO, I, PD, ST
F4C8VDDIN33GPIOPD1I/OAD15–BFLEXCOM11_IO1I/O2PIO, I, PD, ST
H12D15VDDSDMMC2GPIOPD2I/O––ASDMMC2_RSTNO1PIO, I, PU, ST
BPCK0O2
CCANTX4O1
DD7I/O2
ETIOA0I/O2
FFLEXCOM8_IO0I/O5
B15C17VDDSDMMC2HSIOPD3I/O––ASDMMC2_CMDI/O1PIO, I, PU, ST
BFLEXCOM0_IO0I/O2
CCANRX4I1
DNANDRDYI2
ETIOB0I/O2
FFLEXCOM8_IO1I/O5
A15B14VDDSDMMC2HSIOPD4I/O––ASDMMC2_CKO1PIO, I, PU, ST
BFLEXCOM0_IO1I/O2
CCANTX5O1
DNCS3/NANDCSO2
ETCLK0I2
FFLEXCOM9_IO0I/O5
A16C16VDDSDMMC2HSIOPD5I/O––ASDMMC2_DAT0I/O1PIO, I, PU, ST
BFLEXCOM0_IO2I/O2,3
CCANRX5I1
DNWE/NWR0/NANDWEO2
ETIOA1I/O2
FFLEXCOM9_IO1I/O5
G12C15VDDSDMMC2HSIOPD6I/O––ASDMMC2_DAT1I/O1PIO, I, PU, ST
BFLEXCOM0_IO3I/O2,3
CSPDIF_RXI3
DNRD/NANDOEO2
ETIOB1I/O2
FFLEXCOM10_IO0I/O5
J11D14VDDSDMMC2HSIOPD7I/O––ASDMMC2_DAT2I/O1PIO, I, PU, ST
BFLEXCOM0_IO4O2,3
CSPDIF_TXO3
DA21/NANDALEO2
ETCLK1I2
FFLEXCOM10_IO1I/O5
B13B15VDDSDMMC2HSIOPD8I/O––ASDMMC2_DAT3I/O1PIO, I, PU, ST
CI2SMCC0_DIN0I2
DA22/NANDCLEO2
ETIOA2I/O2
FFLEXCOM11_IO0I/O5
D19K19VDDIOP1GPIOPD9I/O––ASDMMC2_WPI1PIO, I, PU, ST
CI2SMCC0_DIN1I2
DD0I/O2
ETIOB2I/O2
FFLEXCOM11_IO1I/O5
M12J18VDDIOP1GPIOPD10I/O––ASDMMC2_CDI1PIO, I, PU, ST
BPCK6O2
CI2SMCC0_DIN2I2
DD1I/O2
ETCLK2I2
FFLEXCOM0_IO0I/O3
A20K20VDDIOP1GPIOPD11I/O––ASDMMC2_1V8SELO1PIO, I, PU, ST
BPCK7O2
CI2SMCC0_DIN3I2
DD2I/O2
ETIOA3I/O2
FFLEXCOM0_IO1I/O3
P12G18VDDIOP1GPIOPD12I/O––APCK1O2PIO, I, PU, ST
BFLEXCOM1_IO0I/O2
DCANTX0O2
ETIOB3I/O2
H18H20VDDIOP1GPIOPD13I/O––AI2SMCC0_CKI/O2PIO, I, PU, ST
BFLEXCOM1_IO1I/O2
CPWML0O4
DCANRX0I2
ETCLK3I2
C19F21VDDIOP1GPIOPD14I/O––AI2SMCC0_MCKO2PIO, I, PU, ST
BFLEXCOM1_IO2I/O2,3,4
CPWMH0O4
DCANTX1O2
ETIOA4I/O2
FFLEXCOM2_IO0I/O5
R12J19VDDIOP1GPIOPD15I/O––AI2SMCC0_WSI/O2PIO, I, PU, ST
BFLEXCOM1_IO3I/O2,3,4
CPWML1O4
DCANRX1I2
ETIOB4I/O2
FFLEXCOM2_IO1I/O5
D18G21VDDIOP1GPIOPD16I/O––AI2SMCC0_DOUT0O2PIO, I, PU, ST
BFLEXCOM1_IO4O2,3,4
CPWMH1O4
DCANTX2O2
ETCLK4I2
FFLEXCOM3_IO0I/O5
G18F18VDDIOP1GPIOPD17I/O––AI2SMCC0_DOUT1O2PIO, I, PU, ST
BFLEXCOM2_IO0I/O2
CPWML2O4
DCANRX2I2
ETIOA5I/O2
FFLEXCOM3_IO1I/O5
B19F20VDDIOP1GPIOPD18I/O––AI2SMCC0_DOUT2O2PIO, I, PU, ST
BFLEXCOM2_IO1I/O2
CPWMH2O4
DCANTX3O2
ETIOB5I/O2
FFLEXCOM4_IO0I/O5
N11G20VDDIOP1GPIOPD19I/O––AI2SMCC0_DOUT3O2PIO, I, PU, ST
BFLEXCOM2_IO2I/O2,3,4,5
CPWML3O4
DCANRX3I2
ETCLK5I2
FFLEXCOM4_IO1I/O5
C18F19VDDIOP1GPIOPD20I/O––APCK0O3PIO, I, PU, ST
BFLEXCOM2_IO3I/O2,3,4,5
CPWMH3O4
DCANTX4O2
FFLEXCOM5_IO0I/O5
F18H19VDDIOP1GPIOPD21I/O––APCK1O3PIO, I, PU, ST
BFLEXCOM2_IO4O2,3,4,5
DCANRX4I2
FFLEXCOM5_IO1I/O5
GG1_TXENO1
A19G19VDDIOP1GPIOPD22I/O––APDMC0_CLKO2PIO, I, PU, ST
CPWMEXTRG0I4
DRD1I2
FCANTX5O2
GG1_TX0O1
K12E20VDDIOP1GPIOPD23I/O––APDMC0_DS0I2PIO, I, PU, ST
CPWMEXTRG1I4
DRF1I/O2
EISC_MCKO2
FCANRX5I2
GG1_TX1O1
D17D21VDDIOP1GPIOPD24I/O––APDMC0_DS1I2PIO, I, PU, ST
CPWMFI0I4
DRK1I/O2
EISC_D0I2
GG1_RXDV/G1_CRSDVI1
K10E18VDDIOP1GPIOPD25I/O––APDMC1_CLKO2PIO, I, PU, ST
BFLEXCOM5_IO0I/O2
CPWMFI1I4
DTD1O2
EISC_D1I2
GG1_RX0I1
G14H18VDDIOP1GPIOPD26I/O––APDMC1_DS0I2PIO, I, PU, ST
BFLEXCOM5_IO1I/O2
CADTRGI3
DTF1I/O2
EISC_D2I2
GG1_RX1I1
D16D19VDDIOP1GPIOPD27I/O––APDMC1_DS1I2PIO, I, PU, ST
BFLEXCOM5_IO2I/O2,3,4,5
CTIOA0I/O3
DTK1I/O2
EISC_D3I2
GG1_RXERI1
J12D16VDDIOP1GPIOPD28I/O––ARD0I2PIO, I, PU, ST
BFLEXCOM5_IO3I/O2,3,4,5
CTIOB0I/O3
DI2SMCC1_CKI/O2
EISC_D4I2
FPWML3O5
GG1_MDCO1
B18D18VDDIOP1GPIOPD29I/O––ARF0I/O2PIO, I, PU, ST
BFLEXCOM5_IO4O2,3,4,5
CTCLK0I3
DI2SMCC1_WSI/O2
EISC_D5I2
FPWMH3O5
GG1_MDIOI/O1
H13E16VDDIOP1GPIOPD30I/O––ARK0I/O2PIO, I, PU, ST
BFLEXCOM6_IO0I/O2
CTIOA1I/O3
DI2SMCC1_MCKO2
EISC_D6I2
FPWMEXTRG0I5
GG1_TXCK/G1_REFCKI/O1
C16C20VDDIOP1GPIOPD31I/O––ATD0O2PIO, I, PU, ST
BFLEXCOM6_IO1I/O2
CTIOB1I/O3
DI2SMCC1_DOUT0O2
EISC_D7I2
FPWMEXTRG1I5
GG1_TX2O1
E18H21VDDIOP1GPIOPE0I/O––ATF0I/O2PIO, I, PU, ST
BFLEXCOM6_IO2I/O2,3,4,5
CTCLK1I3
DI2SMCC1_DOUT1O2
EISC_HSYNCI2
FPWMFI0I5
GG1_TX3O1
F14C21VDDIOP1GPIOPE1I/O––ATK0I/O2PIO, I, PU, ST
BFLEXCOM6_IO3I/O2,3,4,5
CTIOA2I/O3
DI2SMCC1_DOUT2O2
EISC_VSYNCI2
FPWMFI1I5
GG1_RX2I1
A18C19VDDIOP1GPIOPE2I/O––APWML0O5PIO, I, PU, ST
BFLEXCOM6_IO4O2,3,4,5
CTIOB2I/O3
DI2SMCC1_DOUT3O2
EISC_FIELDI2
GG1_RX3I1
C15B20VDDIOP1GPIOPE3I/O––APWMH0O5PIO, I, PU, ST
BFLEXCOM0_IO0I/O4
CTCLK2I3
DI2SMCC1_DIN0I2
EISC_PCKI2
GG1_RXCKI1
D15D17VDDIOP1GPIOPE4I/O––APWML1O5PIO, I, PU, ST
BFLEXCOM0_IO1I/O4
CTIOA3I/O3
DI2SMCC1_DIN1I2
EISC_D8I2
GG1_TXERO1
B16B21VDDIOP1GPIOPE5I/O––APWMH1O5PIO, I, PU, ST
BFLEXCOM0_IO2I/O4
CTIOB3I/O3
DI2SMCC1_DIN2I2
EISC_D9I2
GG1_COLI1
G13E17VDDIOP1GPIOPE6I/O––APWML2O5PIO, I, PU, ST
BFLEXCOM0_IO3I/O4
CTCLK3I3
DI2SMCC1_DIN3I2
EISC_D10I2
GG1_CRSI1
E14E19VDDIOP1GPIOPE7I/O––APWMH2O5PIO, I, PU, ST
BFLEXCOM0_IO4O4
CTIOA4I/O3
EISC_D11I2
GG1_TSUCOMPI1
G6C7ADVREFPReferenceADVREFPI/O–––––––
H3A3VDDIN33PowerVDDIN33––––––––
H1–GNDIN33GroundGNDIN33––––––––
F5–GNDANAGroundGNDANA––––––––
G5–GNDANAGroundGNDANA––––––––
J4–GNDANAGroundGNDANA––––––––
T13U13VDDIOP0PowerVDDIOP0––––––––
W14U14VDDIOP0PowerVDDIOP0––––––––
C14–VDDIOP1PowerVDDIOP1––––––––
C17E21VDDIOP1PowerVDDIOP1––––––––
A11L9GNDGroundGND––––––––
A14L10GNDGroundGND––––––––
A17L11GNDGroundGND––––––––
A21L12GNDGroundGND––––––––
AA1L13GNDGroundGND––––––––
AA8L15GNDGroundGND––––––––
AA11M5GNDGroundGND––––––––
AA14M9GNDGroundGND––––––––
AA17M10GNDGroundGND––––––––
AA21M11GNDGroundGND––––––––
D9M12GNDGroundGND––––––––
D13M13GNDGroundGND––––––––
E5H9VDDANAPowerVDDANA––––––––
E6J9VDDANAPowerVDDANA––––––––
J6A5VDDANAPowerVDDANA––––––––
F6E7VDDCOREPowerVDDCORE––––––––
F9E8VDDCOREPowerVDDCORE––––––––
F15E14VDDCOREPowerVDDCORE––––––––
J9E15VDDCOREPowerVDDCORE––––––––
J13K5VDDCOREPowerVDDCORE––––––––
L3L5VDDCOREPowerVDDCORE––––––––
L19L17VDDCOREPowerVDDCORE––––––––
N13M17VDDCOREPowerVDDCORE––––––––
P19R11VDDCOREPowerVDDCORE––––––––
U16R12VDDCOREPowerVDDCORE––––––––
U17U6VDDCOREPowerVDDCORE––––––––
U19U15VDDCOREPowerVDDCORE––––––––
W17U16VDDCOREPowerVDDCORE––––––––
Y20V6VDDCOREPowerVDDCORE––––––––
B20F17VDDCPUPowerVDDCPU––––––––
E16G15VDDCPUPowerVDDCPU––––––––
E17H15VDDCPUPowerVDDCPU––––––––
E19J17VDDCPUPowerVDDCPU––––––––
F16K17VDDCPUPowerVDDCPU––––––––
E7M15GNDGroundGND––––––––
E15M21GNDGroundGND––––––––
E21N5GNDGroundGND––––––––
F17N9GNDGroundGND––––––––
G11N13GNDGroundGND––––––––
G15N15GNDGroundGND––––––––
G17N17GNDGroundGND––––––––
H8P7GNDGroundGND––––––––
H14P9GNDGroundGND––––––––
H21P13GNDGroundGND––––––––
J18P15GNDGroundGND––––––––
K11R1GNDGroundGND––––––––
L1R7GNDGroundGND––––––––
L7R8GNDGroundGND––––––––
L11R9GNDGroundGND––––––––
L15R10GNDGroundGND––––––––
L21R13GNDGroundGND––––––––
N4R14GNDGroundGND––––––––
A1–GNDUTMIGroundGNDUTMI––––––––
A5–GNDUTMIGroundGNDUTMI––––––––
A8–GNDUTMIGroundGNDUTMI––––––––
E1–GNDUTMIGroundGNDUTMI––––––––
G7–GNDUTMIGroundGNDUTMI––––––––
B2D9VDDUTMIIPowerVDDUTMII––––––––
C5D11VDDUTMIIPowerVDDUTMII––––––––
C8D13VDDUTMIIPowerVDDUTMII––––––––
E3E10VDDUTMIIPowerVDDUTMII––––––––
F7E12VDDUTMIIpowerVDDUTMII––––––––
A3A8VDDUTMIUSBPHYHHSA_DPI/O–––––––
B3A9VDDUTMIUSBPHYHHSA_DMI/O–––––––
D7B11VDDUTMIUSBPHYHHSA_CC1I/O–––––––
G9C11VDDUTMIUSBPHYHHSA_CC2I/O–––––––
C6B8VDDUTMIUSBPHYHHSA_RTUNEI–––––––
A4A11VDDUTMIUSBPHYHHSB_DPI/O–––––––
B4A12VDDUTMIUSBPHYHHSB_DMI/O–––––––
C7B12VDDUTMIUSBPHYHHSB_CC1I/O–––––––
E8C12VDDUTMIUSBPHYHHSB_CC2I/O–––––––
D8B10VDDUTMIUSBPHYHHSB_RTUNEI–––––––
A6A13VDDUTMIUSBPHYHHSC_DPI/O–––––––
B6A14VDDUTMIUSBPHYHHSC_DMI/O–––––––
B7B13VDDUTMIUSBPHYHHSC_RTUNEI–––––––
AA5E5VDDIODDRPowerVDDIODDR––––––––
M11F5VDDIODDRPowerVDDIODDR––––––––
N6G5VDDIODDRPowerVDDIODDR––––––––
N9H7VDDIODDRPowerVDDIODDR––––––––
N12J7VDDIODDRPowerVDDIODDR––––––––
P3M7VDDIODDRPowerVDDIODDR––––––––
P13N7VDDIODDRPowerVDDIODDR––––––––
T6P5VDDIODDRPowerVDDIODDR––––––––
T7R5VDDIODDRPowerVDDIODDR––––––––
T9T5VDDIODDRPowerVDDIODDR––––––––
U3U4VDDIODDRPowerVDDIODDR––––––––
U5U5VDDIODDRPowerVDDIODDR––––––––
U6U8VDDIODDRPowerVDDIODDR––––––––
W8U9VDDIODDRPowerVDDIODDR––––––––
Y2U10VDDIODDRPowerVDDIODDR––––––––
N18R15GNDGroundGND––––––––
P1R17GNDGroundGND––––––––
P8T4GNDGroundGND––––––––
P14T17GNDGroundGND––––––––
P21T19GNDGroundGND––––––––
R5U11GNDGroundGND––––––––
R7U12GNDGroundGND––––––––
R17V4GNDGroundGND––––––––
T5V5GNDGroundGND––––––––
T17V18GNDGroundGND––––––––
U1V20GNDGroundGND––––––––
U7V21GNDGroundGND––––––––
U21W3GNDGroundGND––––––––
V9W19GNDGroundGND––––––––
V13W20GNDgroundGND––––––––
Y1Y1VDDIODDRDDRDDR_VREFI–––––––
N2J2VDDIODDRDDRDDR_D0I/O–––––––
M7G2VDDIODDRDDRDDR_D1I/O–––––––
R3L2VDDIODDRDDRDDR_D2I/O–––––––
M8F2VDDIODDRDDRDDR_D3I/O–––––––
T2L3VDDIODDRDDRDDR_D4I/O–––––––
N8J3VDDIODDRDDRDDR_D5I/O–––––––
T1H2VDDIODDRDDRDDR_D6I/O–––––––
N7K2VDDIODDRDDRDDR_D7I/O–––––––
Y7Y4VDDIODDRDDRDDR_D8I/O–––––––
AA4AA4VDDIODDRDDRDDR_D9I/O–––––––
Y9AA5VDDIODDRDDRDDR_D10I/O–––––––
Y3W2VDDIODDRDDRDDR_D11I/O–––––––
AA7W5VDDIODDRDDRDDR_D12I/O–––––––
AA3Y3VDDIODDRDDRDDR_D13I/O–––––––
W7Y5VDDIODDRDDRDDR_D14I/O–––––––
W3W4VDDIODDRDDRDDR_D15I/O–––––––
W6P2VDDIODDRDDRDDR_A0O–––––––
P6N2VDDIODDRDDRDDR_A1O–––––––
V5R2VDDIODDRDDRDDR_A2O–––––––
V6T2VDDIODDRDDRDDR_A3O–––––––
R6P3VDDIODDRDDRDDR_A4O–––––––
W4R3VDDIODDRDDRDDR_A5O–––––––
P7N3VDDIODDRDDRDDR_A6O–––––––
W2P4VDDIODDRDDRDDR_A7O–––––––
L8U2VDDIODDRDDRDDR_A8O–––––––
V4R4VDDIODDRDDRDDR_A9O–––––––
T3M2VDDIODDRDDRDDR_A10O–––––––
M9V1VDDIODDRDDRDDR_A11O–––––––
P5K4VDDIODDRDDRDDR_A12O–––––––
V2M4VDDIODDRDDRDDR_A13O–––––––
L9V3VDDIODDRDDRDDR_A14O–––––––
R4M1VDDIODDRDDRDDR_A15O–––––––
U4N1VDDIODDRDDRDDR_CLKO–––––––
T4P1VDDIODDRDDRDDR_CLKNO–––––––
V3N4VDDIODDRDDRDDR_CKEO–––––––
V1L4VDDIODDRDDRDDR_RESETNO–––––––
V7V2VDDIODDRDDRDDR_CSNO–––––––
N10U1VDDIODDRDDRDDR_WENO–––––––
U8U3VDDIODDRDDRDDR_RASNO–––––––
T8T1VDDIODDRDDRDDR_CASNO–––––––
N1J1VDDIODDRDDRDDR_DQM0O–––––––
Y4Y2VDDIODDRDDRDDR_DQM1O–––––––
R1H1VDDIODDRDDRDDR_DQS0I/O–––––––
Y6AA2VDDIODDRDDRDDR_DQS1I/O–––––––
R2G1VDDIODDRDDRDDR_DQSN0I/O–––––––
AA6AA3VDDIODDRDDRDDR_DQSN1I/O–––––––
V8W1VDDIODDRDDRDDR_BA0O–––––––
P4L1VDDIODDRDDRDDR_BA1O–––––––
R8T3VDDIODDRDDRDDR_BA2O–––––––
W1M3VDDIODDRDDRDDR_ODTO–––––––
AA2K3VDDIODDRDDRDDR_ZQI–––––––
T15–VDDDPHYPowerVDDDPHY––––––––
T16W16VDDDPHYPowerVDDDPHY––––––––
R15–GNDDPHYGroundGNDDPHY––––––––
U15–GNDDPHYGroundGNDDPHY––––––––
N20AA18VDDDPHYPHYMIPI_CLKNI–––––––
N21AA19VDDDPHYPHYMIPI_CLKPI–––––––
R18Y18VDDDPHYPHYMIPI_DN0I–––––––
P18Y19VDDDPHYPHYMIPI_DP0I–––––––
R20AA16VDDDPHYPHYMIPI_DN1I–––––––
R21AA17VDDDPHYPHYMIPI_DP1I–––––––
R19U17VDDDPHYPHYMIPI_REXTI–––––––
J16N21VDDSDMMC0PowerVDDSDMMC0––––––––
C11A15VDDSDMMC1PowerVDDSDMMC1––––––––
W5Y20GNDGroundGND––––––––
K15N19VDDSDMMC0Calib padSDMMC0_CALI–––––––
J10B17VDDSDMMC1Calib padSDMMC1_CALI–––––––
F13B19VDDSDMMC2PowerVDDSDMMC2––––––––
D14C18VDDSDMMC2Calib padSDMMC2_CALI–––––––
R11–GNDBATGroundGNDBAT––––––––
P11U7VBATPowerVBAT––––––––
AA19Y7VBATPIOBU0I––––––PU(5)
P9W10VBATPIOBU1I––––––PU(5)
AA18W9VBATPIOBU2I––––––PU(5)
P10W7VBATPIOBU3I––––––PD(5)
J2D1VDDIN33XINI–––––––
J1E1VDDIN33XOUTO–––––––
Y13AA7VBATXIN32I–––––––
AA13AA8VBATXOUT32O–––––––
AA9Y6VBATTSTI––––––PD
W15W11VBATJTAGSELI––––––PD
AA15Y8VBATWKUP0I–––––––
R9W6VBATSHDNO–––––––
J7C3VDDIN33NRSTI––––––PU
H4A2VDDIN33NRST_OUTO–––––––
K7F3VDDIN33AUDIOCLKO–––––––
R10W8VBATLPMO–––––––
N16P17VDDQSPI0PowerVDDQSPI0––––––––
P16U18VDDQSPI0Calib padQSPI0_CALI–––––––
H19K21VDDQSPI1PowerVDDQSPI1––––––––
W11AA9GNDGroundGNDI–––––––
–A1GNDGroundGND––––––––
–A10GNDGroundGND––––––––
–A17GNDGroundGND––––––––
–A21GNDGroundGND––––––––
–AA1GNDGroundGND––––––––
–AA6GNDGroundGND––––––––
–AA13GNDGroundGND––––––––
–AA21GNDGroundGND––––––––
–B16GNDGroundGND––––––––
–C1GNDGroundGND––––––––
–C14GNDGroundGND––––––––
–D2GNDGroundGND––––––––
–D20GNDGroundGND––––––––
–E2GNDGroundGND––––––––
–E6GNDGroundGND––––––––
–E9GNDGroundGND––––––––
–E13GNDGroundGND––––––––
–F1GNDGroundGND––––––––
–G7GNDGroundGND––––––––
–G8GNDGroundGND––––––––
–G9GNDGroundGND––––––––
–G10GNDGroundGND––––––––
–G11GNDGroundGND––––––––
–G12GNDGroundGND––––––––
–G13GNDGroundGND––––––––
–G14GNDGroundGND––––––––
–G17GNDGroundGND––––––––
–H4GNDGroundGND––––––––
–H5GNDGroundGND––––––––
–H13GNDGroundGND––––––––
–H17GNDGroundGND––––––––
–J4GNDGroundGND––––––––
–J5GNDGroundGND––––––––
–J13GNDGroundGND––––––––
–J15GNDGroundGND––––––––
–J21GNDGroundGND––––––––
–K1GNDGroundGND––––––––
–K7GNDGroundGND––––––––
–K9GNDGroundGND––––––––
–K10GNDGroundGND––––––––
–K11GNDGroundGND––––––––
–K12GNDGroundGND––––––––
–K13GNDGroundGND––––––––
–K15GNDGroundGND––––––––
–L7GNDGroundGND––––––––
–E11VDDCPUPowerVDDCPU––––––––
Note:
  1. I/Os for each peripheral are grouped into I/O sets, listed in the column "I/O Set". For all peripherals, use I/Os that belong to the same I/O set. Timings can be unpredictable when I/Os from different I/O sets are mixed.
  2. When using an I/O line with the Analog–to–Digital Converter (ADC) or with the Analog Comparator Controller (ACC), the PIO line configuration (pull–up, pull–down) programmed before assigning this line to the ADC or ACC peripheral is not modified by this peripheral.
  3. Refer to the section Electrical Characteristics for further details.
  4. Signal = ‘PIO’ if GPIO; Dir = Direction; PU = Pull–up; PD = Pull–down; HiZ = High impedance; ST = Schmitt Trigger
  5. This is the PIOBU state after VBAT power–up. If programmed to another value, this value is maintained as long as VBAT is not removed.