2.9.2.9.2 Command Format
The commands are formatted as follows:
____,________,________,________,__#
opcode addrxx length not_used rw
where:
opcode—4 characters of the command.addr—the address field is max 8 characters long, and contains the hexadecimal address value without '0x'.length—in case of a write command, this field indicates the size of the data to be sent, in hexadecimal, without '0x'.not_used—this field is not used for the moment.rw—indicates a read or write operation (00 for read, 01 for write).Table 2-28. Simple Commands Command Full Name Description SEMB SET_EXT_MEM_BOOT_EN Set external memory boot enable SKIF SET_KEYS_IN_FUSE Set keys in fuse SPAI SET_PAIRING_MODE Set Pairing mode SMDI SET_MONITOR_DIS Set monitor disable SBSD SET_BSCR_DIS Set BSCR disable SSBD SET_SEC_DBG Set secure debug SJTD SET_JTAG_DIS Set JTAG disable fuse bit CRST(1) CHIP_RESET Reset the chip Note:- USB communication is cut when this command is executed by the chip.
Table 2-29. Read Version Command Command Full Name Description RVER READ_ROM_VERSION Read ROM code version Table 2-30. Key Management Commands Command Full Name Description WCKY WRITE_CUSTOMER_KEY Send customer keys and initialization vector (640 bits) WRHA WRITE_RSA_HASH Send RSA hash of root certificate public key Note: Sending the commands in the table above automatically configures the corresponding values in the SIGN_MODE and EXPAND_MODE fields of the Boot Configuration Word.Table 2-31. Applet Related Commands Command Full Name Description SAPT SEND_APPLET Send memory programming applet SMBX SEND_APPLET_MAILBOX Send applet mailbox content RMBX READ_APPLET_MAILBOX Read applet mailbox content EAPP APPLET_EXECUTE Execute apple SFIL SEND_FILE Send file (to be programmed into an external memory) RFIL READ_FILE Read file from an external memory