9.6.6.12 MCAN Protocol Status Register

Name: MCAN_PSR
Offset: 0x44
Reset: 0x00000707
Property: Read-only

Bit 3130292827262524 
          
Access  
Reset  
Bit 2322212019181716 
  TDCV[6:0] 
Access RRRRRRR 
Reset 0000000 
Bit 15141312111098 
  PXERFDFRBRSRESIDLEC[2:0] 
Access RRRRRRR 
Reset 0000111 
Bit 76543210 
 BOEWEPACT[1:0]LEC[2:0] 
Access RRRRRRRR 
Reset 00000111 

Bits 22:16 – TDCV[6:0] Transmitter Delay Compensation Value

0 to 127: Position of the secondary sample point, in CAN core clock periods, defined by the sum of the measured delay from CANTX to CANRX and MCAN_TDCR.TDCO.

Bit 14 – PXE Protocol Exception Event (cleared on read)

ValueDescription
0

No protocol exception event occurred since last read access

1

Protocol exception event occurred

Bit 13 – RFDF Received a CAN FD Message (cleared on read)

This bit is set independently from acceptance filtering.

ValueDescription
0

Since this bit was reset by the CPU, no CAN FD message has been received

1

Message in CAN FD format with FDF flag set has been received

Bit 12 – RBRS BRS Flag of Last Received CAN FD Message (cleared on read)

This bit is set together with RFDF, independently from acceptance filtering.

ValueDescription
0

Last received CAN FD message did not have its BRS flag set.

1

Last received CAN FD message had its BRS flag set.

Bit 11 – RESI ESI Flag of Last Received CAN FD Message (cleared on read)

This bit is set together with RFDF, independently from acceptance filtering.

ValueDescription
0

Last received CAN FD message did not have its ESI flag set.

1

Last received CAN FD message had its ESI flag set.

Bits 10:8 – DLEC[2:0] Data Phase Last Error Code (set to 111 on read)

Type of last error that occurred in the data phase of a CAN FD format frame with its BRS flag set. Coding is the same as for LEC. This field will be cleared to zero when a CAN FD format frame with its BRS flag set has been transferred (reception or transmission) without error.

Bit 7 – BO Bus_Off Status

ValueDescription
0

The MCAN is not Bus_Off.

1

The MCAN is in Bus_Off state.

Bit 6 – EW Warning Status

ValueDescription
0

Both error counters are below the Error_Warning limit of 96.

1

At least one of error counter has reached the Error_Warning limit of 96.

Bit 5 – EP Error Passive

ValueDescription
0

The MCAN is in the Error_Active state. It normally takes part in bus communication and sends an active error flag when an error has been detected.

1

The MCAN is in the Error_Passive state.

Bits 4:3 – ACT[1:0] Activity

Monitors the CAN communication state of the CAN module.

ValueNameDescription
0 SYNCHRONIZING

Node is synchronizing on CAN communication

1 IDLE

Node is neither receiver nor transmitter

2 RECEIVER

Node is operating as receiver

3 TRANSMITTER

Node is operating as transmitter

Bits 2:0 – LEC[2:0] Last Error Code (set to 111 on read)

The LEC indicates the type of the last error to occur on the CAN bus. This field is cleared when a message has been transferred (reception or transmission) without error.

ValueNameDescription
0 NO_ERROR

No error occurred since LEC has been reset by successful reception or transmission.

1 STUFF_ERROR

More than 5 equal bits in a sequence have occurred in a part of a received message where this is not allowed.

2 FORM_ERROR

A fixed format part of a received frame has the wrong format.

3 ACK_ERROR

The message transmitted by the MCAN was not acknowledged by another node.

4 BIT1_ERROR

During transmission of a message (with the exception of the arbitration field), the device tried to send a recessive level (bit of logical value ‘1’), but the monitored bus value was dominant.

5 BIT0_ERROR

During transmission of a message (or acknowledge bit, or active error flag, or overload flag), the device tried to send a dominant level (data or identifier bit logical value ‘0’), but the monitored bus value was recessive. During Bus_Off recovery, this status is set each time a sequence of 11 recessive bits has been monitored. This enables the processor to monitor the proceeding of the Bus_Off recovery sequence (indicating the bus is not stuck at dominant or continuously disturbed).

6 CRC_ERROR

The CRC check sum of a received message was incorrect. The CRC of an incoming message does not match the CRC calculated from the received data.

7 NO_CHANGE

Any read access to the Protocol Status Register re-initializes the LEC to ‘7’. When the LEC shows value ‘7’, no CAN bus event was detected since the last processor read access to the Protocol Status Register.