14.3.2.4 OSAL_QUEUE_SelectFromSet Function
C
OSAL_RESULT OSAL_QUEUE_SelectFromSet(OSAL_QUEUE_SET_MEMBER_HANDLE_TYPE *queSetMember, OSAL_QUEUE_SET_HANDLE_TYPE *queSetID, uint16_t waitMS);Description
Block to wait for something to be available from the queues or semaphore that have been added to the set.
Parameters
| Param | Description |
|---|---|
| queSetMember | Member queue or semaphore to be added in the set |
| queSetID | A pointer to the queue ID |
| waitMS | wait time in milliseconds. other value OSAL_WAIT_FOREVER |
Returns
OSAL_RESULT_TRUE - A queue had been created
OSAL_RESULT_FALSE - Queue creation failed