1.3.1.1.2 ADPCM_Decoder Function
C
bool ADPCM_Decoder(uint8_t *input, uint16_t inSize, uint16_t *read, int16_t *output, uint16_t *written);Summary
Decode the ADPCM stream of inSize from input pointer into output pointer.
Description
Decode the ADPCM stream of inSize from input pointer into output pointer.
Parameters
inSize - Size of ADPCM input stream in bytes.
read - Size of ADPCM decoder has decoded after this function complete
Returns
output - Pointer to the decoded data.
written - Size of decoded data.
If successful, returns true, otherwise, returns false.
Remarks None.