4.3 Environment Setup
The following steps outline how to set up the environment:
- The user must extract the EV79Y91A package folder.
- Inside the EV79Y91A package folder, locate the
install.shscript. - Double-click the
install.shto run the script. - The
install.shscript generates the Harmony 3 (H3) folder repository.Figure 4-3. Creating H3 Folder - After executing the
install.shscript from the EV79Y91A package folder, it clones all the required H3 repositories. Following this, the H3 repository environment becomes available within the EAP package at \EV79Y91A\H3.Figure 4-4. H3 Repositories - Open the MPLAB® X IDE, then add the Harmony Content Path. Go to Tools>Options>Plugins.
Figure 4-5. Harmony Content Path Note: The Harmony Content Path varies depending on the user’s folder structure. - Click Apply, then Click OK.Note: The user must restart the MPLAB X IDE tool.