1.3.2 Warnings
Read the following warnings before using the Midspan unit:
- Connect the PD-9001GS only to the IP device with which it was bought. Using PD-9001GS with other IP devices can cause damage to the IP device.
- Follow basic electricity safety measures whenever connecting PD-9001GS to its power source.
- A voltage mismatch can cause equipment damage and may pose a fire hazard. If voltage indicated on the label is different from the power outlet voltage, do not connect PD-9001GS to this power outlet.
- Do not use cross-over cable between the PD-9001GS output port and the load device.