2.1 Prerequisites
The following is a list of prerequisites for installing the PoE Midspan unit:
- Read the installation instructions before connecting the PD-9001GS to its power source.
- Apply AC power to the PD-9001GS, using an operational AC cable with an appropriate ground connection.
- Verify that a PoE-ready, Ethernet-compatible device is connected.
- The PD-9001GS can be placed on a desktop. Before placing the PD-9001GS:
- Do not cover PD-9001GS or block airflow to the unit with any foreign objects.
- Keep PD-9001GS away from excessive heat and humidity and free from vibration and dust.
- Ensure that the cable length from Ethernet network source to terminal does not exceed 100 meters (330 feet). This Midspan is not a repeater and does not amplify Ethernet data signal.
- Use a splitter if desired; ensure splitter is connected close to the terminal and not on the PD-9001GS.