3.3 IPK Package Installation
This section describes how to install the demo application onto an existing root filesystem. This method is the fastest way to evaluate the OCPP stack along with the demo application. It also allows you to test a pre-built IPK package directly on a Linux-based target.
Note:
- The IPK package is located in the demo_linux_ocpp_v1.6_certification/ipk folder.
- Ensure that both the target board and the host PC are connected to the same network; otherwise, communication between them will fail.
- The IP
address 10.40.24.185 in the command below must be replaced
with the actual IP address of the target board. To obtain
the target board’s IP address, run the ifconfig
command on the target
board:
root@sama5d27-wlsom1-ek-sd:~# ifconfig eth0 Link encap:Ethernet HWaddr 04:91:62:42:F6:76 inet addr:10.40.24.185 Bcast:10.40.24.255 Mask:255.255.255.0 inet6 addr: fe80::691:62ff:fe43:f675/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:54418 errors:0 dropped:360 overruns:0 frame:0 TX packets:939 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:5176322 (4.9 MiB) TX bytes:63397 (61.9 KiB) Interrupt:156 Base address:0x8000
Once the board has booted successfully and is up and running, execute the commands below on the target board:
- Copy the IPK file
to the target from the host Linux development PC, using a file transfer protocol
such as
SCP:
cd ~demo_linux_ocpp_v1.6_certification/ipk scp demo-ocpp1.6_1.0.0-r0_cortexa5t2hf-neon-vfpv4_2025_10.ipk root@10.40.24.185:/root - Install the IPK
package:
root@sama5d27-wlsom1-ek-sd:~#opkg install demo-ocpp1.6_1.0.0-r0_cortexa5t2hf-neon-vfpv4_2025_10.ipk - Verify the
installation:
root@sama5d27-wlsom1-ek-sd:#ls /ocpp1.6/ CSR.json Invalid_Signed_Cert.pem OCPP_v16.json Signed_Cert.pem certificate.pem chargeingprofilem_v2.db csr_output.pem oflinepackets.db tagauthcache.db CentralSystemRootCertificate.crt ManufacturerRootCertificate.crt PrivateKey.json ca_cert.pem certificates.json config.json ocpp1.6_WD private_key.pem taglocallist.db - Run the OCPP demo
application:
root@sama5d27-wlsom1-ek-sd:/ocpp1.6#./ocpp1.6_WD 2025-12-10 08:47:03 [DEBUG]: [APP_LOG] Options: Reboot the application: 0: Reboot the applicationCore: A: Authorize B: Boot Notification c: Change Configuration D: Data Transfer H: Heart Beat M: Meter Values R: Reset S: StartTransaction N: StatusNotification Z: StopTransaction - Go to OCPP Compliance Test Tool (OCTT) Server Setup.