1.13 SPI Driver Asynchronous - Self Loopback Multi Client
This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients.
Description
- This example writes and reads back the same data (self loop back) for two different clients connected over the same SPI bus by using the multi client feature of the driver
 - It uses the request (write and read request) queuing feature of the asynchronous driver and does not waste CPU bandwidth in waiting for previous request completion
 - The example also demonstrates how to setup two different client transfers at different baud rates
 - This example performs self loop back only once after a power on reset
 - Success is indicated when a successful self loop back is reported by both the clients
 - After the loop back test is complete, the application remains in the idle state
 
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/spi/async/spi_self_loopback_multi_client/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32mz_dag_sk.X | MPLABX project for PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit | 
| pic32mz_das_sk.X | MPLABX project for PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto) | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32mz_dag_sk.X | PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit | 
| pic32mz_das_sk.X | PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto) | 
Setting Up PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
 - Use jumper wire to connect “Pin 21 of J15” to “Pin 19 of J15”
- SDI2 is mapped to RD7 that is routed to “Pin 21 of J15”
 - SDO2 is mapped to RG8 that is routed to “Pin 19 of J15”
 
 
Setting Up PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto)
- Connect the Debug USB port on the board to the computer using a micro USB cable
 - Use jumper wire to connect “Pin 21 of J15” to “Pin 19 of J15”
- SDI2 is mapped to RD7 that is routed to “Pin 21 of J15”
 - SDO2 is mapped to RG8 that is routed to “Pin 19 of J15”
 
 
Running the Application
- Build and program the application using its IDE
 - The LED is turned ON on Success
 
Refer to the following table for LED name: