1 Harmony 3 USB Host application examples
MPLAB® Harmony 3 is an extension of the MPLAB® ecosystem for creating embedded firmware solutions for Microchip 32-bit SAM and PIC® microcontroller and microprocessor devices. Refer to the following links for more information.
- Microchip 32-bit MCUs
- Microchip 32-bit MPUs
- Microchip MPLAB X IDE
- Microchip MPLAB® Harmony
- Microchip MPLAB® Harmony Pages
This repository contains the MPLAB® Harmony 3 USB Host application examples.
To clone or download these applications from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Contents Summary
| Folder | Description |
|---|---|
| apps | Contains Harmony 3 USB Host application examples |
| docs | Contains documentation in html format for offline viewing (to be used only after cloning this repository onto a local machine). Use github pages of this repository for viewing it online. |
Code Examples
The following applications are provided to demonstrate the typical or interesting usage models of USB Host capabilities.
| Name | Description |
|---|---|
| CDC Basic | This application uses the USB Host Layer and CDC Client driver to enumerate a standard CDC USB device. The demonstration host application then operates and uses the functionality of the attached CDC Device. |
| CDC MSD | This application creates a USB Host that can recognize and enumerate a CDC USB Device and MSC USB Device. |
| HID Basic Keyboard | This application creates a USB Host application that uses the USB Host Layer, HID Client driver and HID Keyboard Usage driver to enumerate a USB keyboard and understand keyboard press release events. The keyboard events are displayed using a terminal emulator on a personal computer. |
| HID Basic Mouse USART | This application uses the USB Host layer, HID Client driver and HID Mouse Usage driver to enumerate a USB Mouse and detect Mouse button press release events. The Mouse events are displayed using a terminal emulator on a personal computer. |
| HUB CDC HID | This application creates a USB Host that can recognize and enumerate a CDC Emulator USB Device and a HID USB Mouse connected via an external Hub. The host will demonstrate the communication from the CDC emulator device and the HID mouse. |
| HUB MSD | This application uses USB Host stack and the Harmony Filesystem Service to copy a file from a source USB pen drive to a target USB pen drive. |
| MSD Basic | This application demonstrates the use of the MSD Host Class Driver to write a file to a USB Flash drive. The application uses the USB Host_layer , MSD class driver and the MPLAB Harmony File System Framework to enumerate a USB Flash drive and to write a file to it. |
| ROOT HUB DUAL MSD | This application demonstrates the use of the root hub of the host. |
| Vendor | This application demonstrates how to interface with a USB device using the generic host client driver. |