1.7 MSD Basic Example (msd_basic)
This application demonstrates the ability of the MPLAB Harmony USB Host Stack to support MSD Host Class Driver . It demonstrates the feature with an application to read / write a file to a USB Flash drive.
Description
This application demonstrates the use of the MSD Host Class Driver to write a file to a USB Flash drive. The application uses the USB Host_layer , MSD class driver and the MPLAB Harmony File System Framework to enumerate a USB Flash drive and to write a file to it.
Downloading and building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is usb_apps_host/apps/msd_basic.
Following table gives the details of project configurations, target device used, hardware and its IDE. Open the project using the respective IDE and build it.
| Project Name | IDE | Target Device | Hardware / Configuration |
|---|---|---|---|
| pic32mk_gp_db.X | MPLABX | PIC32MK1024GPE100 | PIC32MK General Purpose (GP) Development Board |
| pic32mk_gp_db_freertos.X | MPLABX | PIC32MK1024GPE100 | PIC32MK General Purpose (GP) Development Board |
| pic32mx470_curiosity.X | MPLABX | PIC32MX470F512H | PIC32MX Curiosity Development Board |
| pic32mx470_curiosity_freertos.X | MPLABX | PIC32MX470F512H | PIC32MX Curiosity Development Board |
| pic32mz_das_sk.X | MPLABX | PIC32MZ2064DAS169 | PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit |
| pic32mz_ef_curiosity_2.X | MPLABX | PIC32MZ2048EFM144 | Curiosity PIC32MZ EF 2.0 Development Board |
| pic32mz_ef_sk.X | MPLABX | PIC32MZ2048EFH144 | PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit |
| pic32mz_ef_sk_freertos.X | MPLABX | PIC32MZ2048EFH144 | PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit |
| pic32mz_w1_curiosity.X | MPLABX | PIC32MZ1025W104132 | Curiosity PIC32MZ W1 Development Board |
| sam_9x60_ek.X | MPLABX | SAM9X60 | SAM9X60-EK Evaluation Board |
| sam_9x60_ek_freertos.X | MPLABX | SAM9X60 | SAM9X60-EK Evaluation Board |
| sam_9x60_curiosity.X | MPLABX | SAM9X60 | SAM9X60 Curiosity Development Board |
| sam_9x60_curiosity_freertos.X | MPLABX | SAM9X60 | SAM9X60 Curiosity Development Board |
| sam_9x75_eb.X | MPLABX | SAM9X75 | SAM9X75-DDR3-EB Evaluation Board |
| sam_a5d2_xult.X | MPLABX | ATSAMA5D27C | SAMA5D2 Xplained Ultra Board |
| sam_a5d2_xult_freertos.X | MPLABX | ATSAMA5D27C | SAMA5D2 Xplained Ultra Board |
| sam_a5d27_som1_ek.X | MPLABX | ATSAMA5D27C | SAMA5D27 SOM1 Kit1 |
| sam_a5d27_som1_ek_freertos.X | MPLABX | ATSAMA5D27C | SAMA5D27 SOM1 Kit1 |
| sam_a5d27_wlsom1_ek1.X | MPLABX | ATSAMA5D27C | ATSAMA5D27 WLSOM1 EK1 |
| sam_a5d27_wlsom1_ek1_freertos.X | MPLABX | ATSAMA5D27C | ATSAMA5D27 WLSOM1 EK1 |
| sam_a7g5_ek.X | MPLABX | SAMA7G54 | SAMA7G5 EK Board |
| sam_d21_xpro.X | MPLABX | ATSAMD21J18A | SAMD21 Xplained Pro Board |
| sam_e54_xpro.X | MPLABX | ATSAME54P20A | SAME54 Xplained Pro Board |
| sam_e70_xult.X | MPLABX | ATSAME70Q21B | SAME70 Xplained Ultra Board |
| sam_e70_xult_freertos.X | MPLABX | ATSAME70Q21B | SAME70 Xplained Ultra Board |
| pic32cz_ca70_curiosity_ultra.X | MPLABX | PIC32CZ2051CA70144 | PIC32CZ CA70 Curiosity Ultra Development Board |
| pic32cz_ca70_curiosity_ultra_freertos.X | MPLABX | PIC32CZ2051CA70144 | PIC32CZ CA70 Curiosity Ultra Development Board |
| sam_g55_xpro.X | MPLABX | ATSAMG55J19 | SAMG55 Xplained Pro Board |
| sam_g55_xpro_freertos.X | MPLABX | ATSAMG55J19 | SAMG55 Xplained Pro Board |
| sam_l21_xpro.X | MPLABX | ATSAML21J18B | SAML21 Xplained Pro Board |
| sam_v71_xult_freertos.X | MPLABX | ATSAMV71Q21B | SAMV71 Xplained Ultra board |
| pic32cz_ca80_curiosity_ultra.X | MPLABX | PIC32CZ8110CA80208 | PIC32CZ Curiosity Development Board |
| pic32cz_ca80_curiosity_ultra_freertos.X | MPLABX | PIC32CZ8110CA80208 | PIC32CZ Curiosity Development Board |
| pic32ck_gc01_curiosity_ultra.X | MPLABX | PIC32CK2051GC01144 | PIC32CK GC Curiosity Ultra Development Board |
| pic32ck_gc01_curiosity_ultra_freertos.X | MPLABX | PIC32CK2051GC01144 | PIC32CK GC Curiosity Ultra Development Board |
| pic32cm_le00_curiosity_pro.X | MPLABX | PIC32CM5164LE00100 | PIC32CM Lx Curiosity Pro Board |
| pic32cx_sg41_curiosity_ultra.X | MPLABX | PIC32CX1025SG41128 | PIC32CX SG41 Curiosity Ultra Evaluation Board |
| sam_a5d29_curiosity.X | MPLABX | ATSAMA5D29 | SAMA5D29 Curiosity Development Board |
| sam_9x75_curiosity.X | MPLABX | SAM9X75D2G | SAM9X75-Curiosity Development Board |
| sam_a7d65_curiosity.X | MPLABX | SAMA7D65 | SAMA7D65 Curiosity Development Board |
| pic32wm_bz6_curiosity.X | MPLABX | PIC32WM_BZ6204 | PIC32WM BZ6 Curiosity Board |
| pic32cm_gc_curiosity_pro.X | MPLABX | PIC32CM5112GC00100 | PIC32CM GC Curiosity Pro Board |
| pic32cm_gc_curiosity_pro_freertos.X | MPLABX | PIC32CM5112GC00100 | PIC32CM GC Curiosity Pro Board |
Configuring the Hardware
- Connect the USB device to the micro-B connector (J102) using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED1 indicates the file write is complete.
- Connect the USB device to the micro-B connector (J200) using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED1 indicates the file write is complete.
- An external power supply (6.5V to 14V) must be connected through the J200 connector.
- Connect the USB device to the Type-C connector (J202).
- LED1 indicates the file write is complete
- Powered the board by connecting an host to "DEBUG USB" (J300) connector.
- Connect the USB device to the USB Host "TARGET USB" (J200) using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED1 indicates the file write is complete.
- Connect the USB device to the "TARGET USB" connector (J201) using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED1 indicates the file write is complete.
- Install a jumper in the J13 header to drive the VBUS line in Host mode.
- Connect the USB device to the USB micro-AB connector J12 using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED1 indicates the file write is complete.
- Connect the USB device to the Type-A connector J5, which is located on the top side of the starter kit.
- LED1 indicates the file write is complete.
- Connect the USB device to the Type-A connector J5, which is located on the top side of the starter kit.
- LED1 indicates the file write is complete.
- Connect the USB device to the Type-A connector J7, which is located on the top side of the starter kit.
- LED1 indicates the file write is complete.
- The jumper titled "PA03 SELECT" must be shorted between PA03 and USB_ID (positions 2 and 3).
- Connect the USB device to the "TARGET USB" connector using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED0 indicates the file write
is complete.Note: An unexpected behavior may be observed if the attached USB device draws an excess amount of current from the board and the Vdd voltage drops below 2.7 volts. The demo has the wait states (NVM_CTRLB <RWS[3:0]>) value set to '1'.
- Connect the USB device to the "TARGET USB" connector using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED0 indicates the file write is complete.
- Jumper J203 must be shorted between PB08 and LED2 (positions 1 and 2).
- Connect the USB device to the "TARGET USB" connector (J200) using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED3 indicates the file write is complete.
- An external power supply (6.5V to 14V) must be connected through the J200 connector.
- Connect the USB device to the "TARGET USB" connector (J203) using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED1 indicates the file write is complete.
- Chip Erase Jumper must be open.
- Connect the USB device to the "TARGET USB" connector using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED0 indicates the file write is complete.
- Connect the USB device to the "TARGET USB" connector using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED0 indicates the file write is complete.
- Jumper titled "USB VBUS" must be shorted between PC09 and LED1 (positions 1 and 2)
- Connect the USB device to the "TARGET USB" connector using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED0 indicates the file write is complete.
- Jumper J205 must be shorted.
- Connect the USB device to the "TARGET USB" connector using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- The LED D204 indicates the file write is complete.
- J205 must be shorted for the Device Functionality.
- Jumper on the pin J211 must
be placed between pin 1 and pin 2.

- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SDMMC connector J4 on the board.
- Reset the board by pressing the Push Button SW3.
- Jumpers J20, J21, and J13 must be open.
- Jumper J2 and J3 must be shorted.
- Connect the USB Micro-B port J22 on board to the computer using a micro USB cable (to enable debug com port).
- Connect the USB Micro-B Connector (J7) on the board to the computer using a micro USB cable to power up the board.
- Connect the USB device to the Type-A connector (J8).
- LED D1 indicates the file write
is complete.

- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SDMMC0 connector J3 on the board.
- Reset the board by pressing the Push Button RESET.
- Jumper J4 must be shorted.
- Connect the USB Micro-B Connector (J1) on the board to the computer using a micro USB cable.
- Connect the USB device to the Type-A connector (J10).
- LED D1 on the board indicates
the file write is complete.

- Powered the board with an external power supply (or use the micro AB connector).
- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SDMMC connector (SDMMC0) on the board.
- Reset the board by pressing the Push Button RESET, then START.
- Connect an USB to serial cable to DBGU0 (to enable debug com port).
- Connect the USB device to the Type-A connector or to the micro AB with a specific dongle (in these case the need to be powered by the external power supply).
- LED near VDDCORE inscription on
the board indicates the file write is complete.

- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SDMMC1 slot on the board.
- Reset the board by pressing the Push Button BP3.
- Connect the EDBG USB Micro-B port J14 on the board to the computer using a micro USB cable.
- Connect the USB device to the USB Type-A connector "A5-USB-B" (J13).
- RGB LED turning to Green indicates the file write is complete.
- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SDMMC0 slot (J12) on the board.
- Reset the board by pressing the Push Button PB1.
- Connect the Debug USB port (J10) on the board to the computer using a micro USB cable.
- Connect the USB device to the USB-B Type-C connector (J19) on the board.
- RGB LED turning to Green
indicates the file write is complete.

- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SD Card Connector (J4) on the board.
- Reset the board by pressing the Reset Button (nRST)
- Connect the USB-A Micro AB connector (J10) on the board to the computer using a micro USB cable.
- Press the "START_SOM" button to activate board start-up.
- Connect the USB device to the USB Type-A connector (J11) on the board.
- RGB LED turning to Green
indicates the file write is complete.

- Powered the board with an external power supply (J1).
- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SD Card Connector (J4) on the board.
- Reset the board by pressing the Reset Button (nRST)
- Press the "nSTART" button to activate board start-up.
- Connect the USB device to the USB Host Type-A connector (J9) on the board. Alternatively, the USB Device could be connected to the Type-C connector (J8) or micro A/B connector (J7).
- RGB LED turning to Green indicates the file write is complete.
- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the μSD-CARD connector J6 on the board.(This connector is present on the bottom face of the board)
- Reset the board by pressing the Push Button RESET.
- Press the "START" button to activate board start-up.
- Connect the USB device to the USB_B Type-A connector (J11) on the board.
- RGB LED (D5) turning to Green indicates the file write is complete.

SAM9X75-Curiosity Development Board
- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the μSD-CARD connector (J14) on the board.(This connector is present on the bottom face of the board)
- Reset the board by pressing the Push Button RESET.
- Press the "START" button to activate board start-up.
- Connect the USB device to the USB_B Type-A connector (J15) or USB_C Type-A connector (J16) on the board.
- RGB LED (LD1) turning to Green indicates the file write is complete.

- Setup the SD card (Note: exFAT
formatted SD Cards are not supported)
- Download harmony MPU bootstrap loader from this location.
- Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
- Insert the SD card into the SD-CARD connector (J10) on the board.
- Reset the board by pressing the Push Button RESET.
- Press the "START" button to activate board start-up.
- Connect the USB device to the USB_B Type-A connector (J23) or USB_C Type-A connector (J24) on the board.
- RGB LED turning to Green indicates the file write is complete.

- Connect a Type-C cable between the DBG USB (J100) port on the board and the PC to power up the board.
- The Jumper J102 must be shorted between 5V and VBUS.
- The Jumper J104 must be connected between VBUSON and EN (Positions 2 and 3).
- Connect the USB device to the USB Type-C connector TARGET USB (J103). A USB Type-C to Type-A Female adapter is required to connect the USB device to the board (This adapter is not included in the kit).
- The RGB_LED (D800) turning Green indicates the file write is complete.

- Connect the USB device to the micro-B connector (J200) using a USB Type-A Female to micro-B male cable (This cable is not included in the kit).
- LED1 indicates the file write is complete.
Running the Application
This application demonstrates the use of the MSD Host Class Driver to write a file to USB Flash drive. The application uses the USB Host_layer, MSD class driver and the MPLAB Harmony File System Framework to enumerate a USB Flash drive and to write a file to it.
- Open the project with appropriate IDE. Compile the project and program the target device.
- With the code running, attach a USB Flash drive to the Host connector on the desired starter kit.
- The demonstration application will then create a file named file.txt. It will then write the text "Hello World" to this file, and then close the file.
- The LED on the selected hardware will indicate the status of the operation. Refer to the Configuring the Hardware instruction for details.
- The USB Flash drive can then be attached to a USB Host personal computer to verify the demonstration application operation.
- Steps 3 through 6 can be repeated.
- If the USB Flash drive already contains a file with the name file.txt, the demonstration application will append the text "Hello World" to the end of the file contents.