32.2.4.1.4 I2C Host Mode Repeated Start Condition Timing
A Repeated Start condition (see Figure 32-26) occurs when the Repeated Start Condition
                  Enable (RSEN)
                  bit is programmed high and the host state machine is Idle. When the RSEN bit is
                  set, the SCL pin is asserted low. When the SCL pin is sampled low, the Baud Rate
                  Generator is loaded and begins counting. The SDA pin is released (brought high)
                  for one Baud Rate Generator count (TBRG). When the Baud Rate Generator
                  times out, if SDA is sampled high, the SCL pin will be deasserted (brought high).
                  When SCL is sampled high, the Baud Rate Generator is reloaded and begins counting.
                  SDA and SCL must remain high for one TBRG. Module hardware then pulls
                  the SDA line low (while SCL remains high) for one TBRG and then pulls
                  the SCL line low. Following this, the RSEN bit will be automatically cleared and
                  the Baud Rate Generator will not be reloaded, leaving the SDA pin held low. As
                  soon as a Start condition is detected on the SDA and SCL pins, the S bit will be set. The SSPxIF bit will not be set until the Baud
                  Rate Generator has timed out.
      Important: 
                  
            - If RSEN is programmed while any other event is in progress, it will not take effect.
- A bus collision during the Repeated Start
                              condition occurs if:- SDA is sampled low when SCL goes from low-to-high.
- SCL goes low before SDA is asserted
                                          low. This may indicate that another host is attempting to
                                          transmit a data ‘1’.