2.6.1 Non-Read-While-Write Area of Flash Not Functional
The Non-Read-While-Write area of the Flash is not working as expected. The problem relates to the device speed when reading the Flash in this area.
Work Around
- Only use the first 248 KB of the Flash
- If boot functionality is needed, run the code in the Non-Read-While-Write area at a maximum of 1/4th of the maximum device frequency at any given voltage by writing the CLKPR register before entering the boot section in the code.
Affected Silicon Revisions
| ATmega2560/2561 | |||
|---|---|---|---|
| Rev. A | Rev. C | Rev. E | Rev. F |
| X | - | - | - |