3.5.1 Read
The following table provides the command syntax for read eFuse before initialization.
| Command Syntax | MCHPRT r | |||||
|---|---|---|---|---|---|---|
| r |
| |||||
| Example | MCHPRT r eFuse information display | |||||
The following figure shows the example of read eFuse before initialization.

The following table provides the command syntax for read eFuse after initialization.
| Command Syntax | MCHPRT 16 r | |||||
|---|---|---|---|---|---|---|
| Example | MCHPRT 16 r eFuse information display | |||||
The following figure shows the example of read eFuse after initialization.