3.4.3 Dump
The following table provides the command syntax for Reg value dump before initialization.
| Command Syntax | MCHPRT REGD X Y F | |||||
|---|---|---|---|---|---|---|
| REGD |
| |||||
| X | X refers to the register number that reads the register value | |||||
| Y | Y refers to the stop register number that reads the register value | |||||
| F | F refers to the register information
file name Example: | |||||
| Example | MCHPRT REGD 0 10
test.txt Report the RX RSSI reading in 10 sec | |||||
The following figure shows the example of reg value dump before initialization.

The following table provides the command syntax for Reg value dump after initialization.
| Command Syntax | MCHPRT 16 REGD X Y F | |||||
|---|---|---|---|---|---|---|
| X | X refers to the register number that reads the register value | |||||
| Y | Y refers to the stop register number that reads the register value | |||||
| F | F refers to the register information
file name Example: | |||||
| Example | MCHPRT 16 REGD 0 10
test.txt Report the RX RSSI reading in 10 sec | |||||
The following figure shows the example of reg value dump after initialization.