9.3 Device Response to a Write Operation Within an Enabled ROM Zone
The AT21CS01/AT21CS11 will respond differently to
a write operation in a memory zone that has been set to ROM in comparison with a write
operation in a memory zone that has not been set to ROM. Writing to the EEPROM is
accomplished by sending a Start condition, followed by a device address byte with the
opcode of 1010b (Ah), the appropriate client address combination, and the
Read/Write bit set as a logic ‘0’. Since a
memory address has not been input at this point in the sequence, the device returns an ACK.
Next, the 8‑bit word address is sent, which will result in an ACK from the device,
regardless of whether that address is in a memory zone that has been set to ROM or not.
However, upon sending the data input byte, a write operation to an address that is in a
memory zone that is set to ROM will result in a NACK response from the AT21CS01/AT21CS11, and the device will be immediately ready to accept a new
command. If the address being written is in a memory zone that has not been set to ROM, the
device will return an ACK to the data input byte as per normal operation for write
operations as described in Write Operations.