8 Read Operations
Read operations are initiated in a similar way as write operations with
the exception that the Read/Write select bit in the device address
byte must be set to a logic ‘1’. There are multiple read operations
supported by the device:
- Current Address Read within the EEPROM
- Random Read within the EEPROM
- Sequential Read within the EEPROM
- Read from the Security Register
- Manufacturer ID Read
If the end of the EEPROM or the Security register is reached, then the Address Pointer will “roll over” to the beginning address of that region. The Address Pointer retains its value between operations as long as the pull-up voltage on the SI/O pin is maintained or as long as the device has not been reset.