9.5.1 Restricted/Unrestricted Secure Erase

For the Sanitize erase patterns (Overwrite, Block Erase, Crypto Scramble), the following erase methods are applicable if your drive supports the method:

  • Restricted: the drive will be unusable until the sanitize operation is completed successfully. If a restricted sanitize operation fails, you are only allowed to start another sanitize operation.

  • Unrestricted: the drive will be recoverable in the case that the sanitize erase operation fails. Data may still be present on the drive. Not all drives support this sanitize method.

For more information about Sanitize erase patterns, see Erasing a Physical Drive.