6.3 Assigning a Dedicated Hot Spare
A dedicated hot spare is assigned to one or more arrays. It will protect any redundant logical drive on those arrays.
Note: You must create
the array before you can assign a dedicated hot spare to protect
it.
To assign a dedicated spare:
- In the Enterprise View, select a controller, an array on that controller, or a Ready physical drive.
-
On the ribbon, in the Physical Device group, click Spare
Management.The Spare Management wizard opens.
-
Select the Dedicated spare type, then click
Next.
-
If you selected a physical drive in the Enterprise view, select the arrays you want to
protect with a dedicated spare, then click Next.
- If you selected an array in the Enterprise view, select the physical drive(s) you want to dedicate as hot spares, then click Next. (See Hot Spare Limitations for help selecting drives.)
- Review the summary of dedicated spares and protected arrays, then click Finish.