9.3.2 Clearing Error Counters from a Controller

Use this option to clear the device error counters of all the physical devices from controller.

To clear the the device errors from a controller:
  1. In the Enterprise View, select the controller node.
  2. On the ribbon, in the Physical Device group, click Set Properties.
    The Set Properties window opens.
  3. To clear the device errors, select the Clear Device Error Counter(s) check box.
  4. Click OK.