10.7.1 Rescanning a Controller

After you connect a physical drive or remove a Ready (non-failed) physical drive from a controller, maxView Storage Manager may not recognize the change until it rescans the controller.

To rescan a controller:

  1. In the Enterprise View, select the controller.
  2. On the ribbon, in the Controller group, click Rescan.
    The Rescan window opens.
  3. Click the Rescan button (on the Rescan window).
    maxView Storage Manager scans all the channels or ports on the controller you selected.
  4. When the rescan is finished, a success message is displayed. Click OK to close the Rescan window.