10.4.2 Setting a Physical Drive to ‘Failed’

Before you can remove a physical drive, you should set it to the Failed state to protect your data. To fail a physical drive (or NVMe SSD), use the Force Offline option for physical devices.

You can set a physical drive to the Failed state if:
  • The physical drive is not part of a logical drive, or
  • The physical drive is part of a redundant, healthy logical drive

Once you force a drive offline, it can be brought online again only after power-cycling the controller.

CAUTION: You may lose data or damage your physical drive if you remove a physical drive without first setting it to a failed state.

To set a physical drive to Failed:

  1. In the Enterprise View, select a controller then, in the Physical Devices tree, select the drive you want to set to Failed.
  2. On the ribbon, in the Physical Devices group, click Force Offline.
    The Force Offline window opens.
  3. Click Force.

    The drive is taken offline and set to the Failed state.

    Note: If the drive is part of a healthy logical drive, the drive is degraded and a warning message is displayed in the Event Log.