26.6.3 Output Pins
The SUPC can drive two outputs. By writing a '1' to the corresponding Output Enable bit in the Backup Output Control register (BKOUT.EN), the SUPC_OUTn pin is driven by the SUPC.
The OUT pin can be set by writing a '1' to the corresponding Set Output bit in the Backup Output Control register (BKOUT.SETx). The OUT pin can be cleared by writing a '1' to the corresponding CLR bit (BKOUT.CLRx).
If the “Toggle Output Mode X is set to “RTCTGL”, the corresponding SUPC_OUTn pin will toggle when an RTC event occurs. Note that before configuring this mode, this is recommended to configure the RTC module properly. If the “Toggle Output Mode X is set to “BKUPTGL”, the corresponding SUPC_OUTn pin will toggle to one when the device goes to Backup Mode. It will toggle to zero when exiting Backup Mode.