5.6.3 Move Logical Device
To a New Array
When the Array status is OK, moving a logical device with new set of SED drives is not allowed based on the following physical device SED security status and SED qualification status:
|
SED Security Status |
SED Qualification Status |
|---|---|
| Locked |
Not Applicable |
|
Not Applicable |
Failed Locking Enabled |
|
Not Applicable |
Failed Range Length Set |
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device Original Factory State (OFS) and SED ownership status:
| Original Factory State (OFS) | SED Ownership Status |
|---|---|
| False | Otherwise Owned |
| False | MCHP Owned, Foreign |
| False | Otherwise Owned, Foreign |
To an Existing Array
Move logical device to an existing array operation on logical device will be blocked when the Array has the following status:
|
Array Status |
|---|
| One or more logical drives undergoing or failed SED qualification |
| Has Logical Drive with Foreign SED |
|
Logical Device Status |
|---|
| SED Qual Failed |
|
SED Qual In Progress |
| SED Locked |