5.6.5 maxCache
On Existing Array
Create logical device operation on an existing array is blocked when the target Array has the following status:
|
Array Status |
|---|
| One or more logical drives undergoing or failed SED qualification |
| Has Logical Drive with Foreign SED |
Create maxCache operation on existing cache array should be blocked when the target Array has the following status:
| Cache Array SED Encryption Status | Logical Device SED Encryption Status |
|---|---|
| Encrypted=True | Encrypted=False |
| Encrypted=False | Encrypted=True |
On New Array
The SED drives can be included in the new Array creation based on the following physical device SED security and SED qualification status.
| SED Security Status | SED Qualification Status |
|---|---|
| Locked |
Not Applicable |
|
Not Applicable |
Failed Locking Enabled |
|
Not Applicable |
Failed Range Length Set |
When the Array status is OK, adding the SED drives to the array is not allowed based on the physical device Original Factory State (OFS) and SED ownership status:
| Original Factory State (OFS) | SED Ownership Status |
|---|---|
| False | Otherwise Owned |
| False | MCHP Owned, Foreign |
| False | Otherwise Owned, Foreign |