12.10.6 Changing the Maximum PCIe Data Rate Settings
The Maximum PCIe Data Rate displays the maximum PCIe data rate between the controller and
the drives connected to the connector. This setting allows to change the maximum PCIe
data rate of the connector on Adaptec Smart Storage Controller. The supported values are
PCIe 3.0, PCIe 4.0, and PCIe 5.0.
Note: The maximum PCIe data rate
will be displayed only if it is supported by the controller. A reboot is required
for the new maximum PCIe data rate to take effect.
To change the Maximum PCIe Data Rate settings:
- In the Enterprise View, select a controller.
- On the ribbon, in the Controller
group, click Set Properties.

The Set Properties window opens.
- Click the Maximum PCIe Data Rate on the
Connector tab. Set the maximum PCIe data rate setting
for each of connector to PCIe 3.0, PCIe 4.0 or PCIe 5.0 from the drop-down list.
To change the maximum PCIe data rate setting for all connectors, select the
desired maximum PCIe data rate from the All Connectors drop-down
list.

- Click OK.
- Reboot the server.