12.10.3 Changing the Connector Operating Mode
- HBA Mode: exposes physical drives to the operating system
- RAID Mode: exposes only RAID volumes to the operating system
- Mixed Mode: exposes RAID volumes and physical drives to the operating system
By default, products with RAID support are configured to operate in Mixed Mode. Mode options vary, depending on the configuration of logical and physical devices on the connector. For example, you cannot switch the connector to HBA mode if the connector is already configured with a RAID volume.
A reboot is required for connector mode changes to take effect.
Note: Changing from Mixed Mode or HBA Mode to RAID Mode
removes access to the physical drives from the operating
system.
To change the connector mode on a controller:
- In the Enterprise View, select a controller.
-
On the ribbon, in the Controller group, click Set
Properties.
When the Set Properties window opens, click the Connector tab. -
From the drop-down list, change the connector mode for each port
to RAID, HBA, or Mixed.

- Click OK.
- Reboot the server.