15.3 Recovering from a Disk Drive Failure
This section describes how to recover when a disk drive or SSD fails:
- If the logical drive is protected by a hot spare, see Failed Disk Drive Protected by a Hot Spare.
- If the logical drive is not protected by a hot spare, see Failed Disk Drive Not Protected by a Hot Spare.
- If there is a disk drive failure in more than one logical drive simultaneously, see Failure in Multiple Logical Drives Simultaneously.
- If it is a RAID 0 logical drive, see Disk Drive Failure in a RAID 0 Logical Drive.
- If multiple disk drives fail within the same logical drive, see Forcing a Logical Drive with Multiple Drive Failures Back Online.