15.3.3 Failure in Multiple Logical Drives Simultaneously
- A hot spare must be at least as big as the smallest disk drive in the array that it might replace.
- Failed disk drives are replaced with hot spares in the order in which they failed. (The logical drive that includes the disk drive that failed first is rebuilt first, assuming an appropriate hot spare is available—see the previous bullet.)
Note: If the number of disk drive
failures exceeds the number of hot spares, see Failed Disk Drive Not Protected by a Hot
Spare..