12.3.1 Locating Disk Drives
To locate an individual disk drive or all physical drives on the controller:
- In the Enterprise View, select a controller or an individual drive on the controller.
-
On the ribbon, in the Physical Device group, click
Locate.
The Locate Physical Device window opens. - From the drop-down list, select the timeout period (1 hour, 4 hours, 24 hours).
-
Click the Locate button.
The LED on the disk drive(s) begin to blink.
-
To stop blinking the drive(s) immediately, click
Stop.

-
Click Cancel to close the Locate Physical
Device window.
The LED(s) continue to blink for the duration of the timeout period.