14.2.4 Changing the Auto-Discovery Settings
Auto-discovery, in maxView Storage Manager, is disabled by default. If enabled, the auto-discovery task runs in the background each time maxView Storage Manager is started. You can enable the auto-discovery if desired, and configure the auto-discovery settings as described in this section.
To change the auto-discovery settings on a system:
- Select the Enterprise view node.
- On the ribbon, in the System group, click System Settings.

The System Settings window opens for that system. The auto-discovery settings appears under General tab..

- To enable/disable auto-discovery, select Enable Auto Discovery. (This option toggles between enabled and disabled.)
- Update the auto-discovery settings. In the Auto Discovery Interval field, enter the number of seconds between each auto-discovery check. This number determines how often maxView Storage Manager checks for changes in remote system resources.
- Click OK to save the changes.