18.3.1 maxView vSphere Plugin Resources

The following section describes the controller details of the maxView vSphere plugin.

The controller has the following three tabs:

  • Summary
  • Device Alert
  • Event

Summary Tab

The Summary tab displays the status and the properties of the resource.

Device Alert Tab

The Device Alert tab display the information(s), warning(s) and errors(s) of the resource.

Event Tab

Event tab provides at-a-glance status information about activity (or events) occurring in the node. All Information, Error, and Warning level events are recorded.

Note:

You can also obtain the similar details of an Array, Enclosure, Event, Logical Device, and Physical device by clicking on the respective tabs.