4 SAM9X60
| No. | Title/Link |
Hardware Board/ Kit Used | Description |
|---|---|---|---|
| 1 | Developing Applications with MPLAB Harmony v3 Software Framework for MPUs | N/A | Step-by-step guide explaining:
|
| 2 | SAM9X60 Boot Process Training Module | SAM9X60 | Boot process of the SAM9X60 microprocessors (MPUs) |
| 3 | MPLAB Discover Code Examples | SAM9X60 | MPLAB Discover code examples |
| 4 | MPLAB github Examples | SAM9X60 | MPLAB Harmony v3 application examples (CSP, Graphics, Ethernet, etc.) |
| 5 | Getting Started on Graphics Application | SAM9X60-Curiosity development board | Step-by-step guide on how to get started developing a graphics application with the SAM9X60-Curiosity development board on MPLAB X IDE |
| 6 | Consumer Graphics (Snake Game) | SAM9X60-Curiosity development board | Snake game application on SAM9X60-Curiosity development board using MPLAB X IDE |
| 7 | SAM9X60 Curiosity Development Board - Introduction | SAM9X60-Curiosity development board | Introduction to the SAM9X60-Curiosity development board |
| 8 | SAM9X60 Curiosity Development Board Features | SAM9X60-Curiosity development board | Features of the SAM9X60 Curiosity Development Board (EV40E67A) |
| 9 | SAM9X60 Curiosity Development Board - Comparison | SAM9X60-Curiosity development board | Feature-by-feature comparison between the SAM9X60-Curiosity development board and the SAM9X60-EK evaluation kit |
| 10 | Booting Demo Linux Image | SAM9X60-Curiosity development board | Step-by-step instructions for booting a demo Linux image from an SD card |
| 11 | Getting started on Linux OS development with SAM9X60-Curiosity Development Board | SAM9X60-Curiosity development board | How to get started on Linux OS development on the SAM9X60-Curiosity development board |
| 12 | Configuring and Building at91bootstrap for an MPLAB Harmony 3 Project Using MPLAB X IDE | SAM9X60-Curiosity development board | Step-by-step guide on how to configure and build at91bootstrap with MPLAB X IDE to debug a Harmony application on MPLAB X IDE |
| 13 | Migration Guide | SAM9X60-Curiosity development board | Migrating an MPLAB Harmony 3 application from SAM9X60-EK to SAM9X60-Curiosity: rtt_periodic_timeout |
| 14 | Getting Started With Graphics on SAM9X60 Curiosity Development Board YouTube video | SAM9X60-Curiosity development board | Step-by-step guide showing customers how to get started with a Harmony-based graphics application on the SAM9X60-Curiosity development board |
| 15 | Getting Started with MPLAB Harmony v3 Development | SAM9X60-Curiosity development board | Step-by-step guide showing how to get started with a Harmony-based application on the SAM9X60-Curiosity development board and debug using PICkit5 |
| 16 | Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from NAND Flash Memory | SAM9X60-Curiosity development board | Step-by-step guide showing how to configure and build at91bootstrap to load an MPLAB Harmony v3 application from a NAND Flash memory |
| 17 | Writing MPLAB Harmony v3 Application and at91bootstrap to NAND Flash Memory using SAM-BA ISP | SAM9X60-Curiosity development board | Step-by-step guide showing how to write an MPLAB Harmony v3 application and at91bootstrap to a NAND Flash memory using SAM-BA ISP |
| 18 | at91bootstrap: Create a Custom Board Configuration | N/A | Customizing a default configuration of at91bootstrap and build at91bootstrap under Linux |
| 19 | at91bootstrap: Customizing a Default Configuration | N/A | How to create a custom board configuration (almost from scratch) for the at91bootstrap bootloader |
| 20 | SAM-BA In-System Programmer (ISP) | N/A | Description of SAM-BA ISP and command line interface |
| 21 | N/A | Application note describing how to get started on Linux OS development | |
| 22 | SAM9X60-EK Evaluation Kit - Introduction | SAM9X60-EK | Introduction to the SAM9X60-EK board |
| 23 | SAM9X60-EK Evaluation Kit - Features | SAM9X60-EK | Features of the SAM9X60-EK Evaluation Kit (DT100126) |
| 24 | SAM9X60-EK Evaluation Kit - Booting a Demo Linux Image | SAM9X60-EK | Booting demo Linux image from an SD card for the SAM9X60-EK board |
| 25 | Booting a Linux Image from NAND Flash Memory | SAM9X60-EK | Step-by-step instructions on how to configure and program at91 and u-boot to boot from a NAND Flash memory |
| 26 | Booting a Linux Image from QSPI Flash Memory | SAM9X60-EK | Step-by-step instructions on how to configure and program at91 and u-boot to boot from a QSPI NOR Flash memory |
| 27 | Booting a Linux Image from SD Memory Card | SAM9X60-EK | Step-by-step instructions on how to configure and program at91 and u-boot to boot from an SD card |
| 28 | Fast Boot Demonstration | SAM9X60-EK | Provides some essential tips and techniques to achieve a quick boot on SAM9X60-EK |
| 29 | Getting Started with MPLAB Harmony v3 Development | SAM9X60-EK | How to get started with MPLAB Harmony v3 application development using rtt_periodic_interrupt |
| 30 | Configure and Build at91bootstrap for an MPLAB Harmony 3 Project with MPLAB X IDE | SAM9X60-EK | How to configure and build at91bootstrap for an MPLAB Harmony 3 project with MPLAB X IDE |
| 31 | Configure and Build at91bootstrap to Load an MPLAB Harmony 3 Application from NAND Flash Memory | SAM9X60-EK | How to configure and build at91bootstrap to load an MPLAB Harmony 3 application from a NAND Flash memory |
| 32 | Writing MPLAB Harmony 3 Application and at91bootstrap to NAND Flash Memory Using SAM-BA ISP | SAM9X60-EK | How to write an MPLAB Harmony 3 application and at91bootstrap to a NAND Flash memory using SAM-BA ISP |
| 33 | Configure and Build at91bootstrap to Load an MPLAB Harmony 3 Application from NOR Flash (QSPI) Memory | SAM9X60-EK | How to configure and build at91bootstrap to load an MPLAB Harmony 3 application from a QSPI NOR Flash memory |
| 34 | Writing MPLAB Harmony 3 Application and at91bootstrap to NOR Flash (QSPI) Memory using SAM-BA ISP | SAM9X60-EK | How to write an MPLAB Harmony 3 application and at91bootstrap to a QSPI NOR Flash memory using SAM-BA ISP |
| 35 | Configure and Build at91bootstrap to Load an MPLAB Harmony 3 Application from SD Memory Card | SAM9X60-EK | How to configure and build at91bootstrap to load an MPLAB Harmony 3 application from an SD card Flash memory |
| 36 | Copy MPLAB Harmony 3 Application and at91bootstrap to SD Memory Card | SAM9X60-EK | How to write an MPLAB Harmony 3 application and at91bootstrap to an SD card |
| 37 | Ensemble Graphics Toolkit: First Application Using Eclipse IDE™ | SAM9X60-EK | How to prepare a host PC (native Linux PC) and target (SAM9X60-EK) to develop applications using the Ensemble Graphics Toolkit (EGT) with Eclipse IDE |
| 38 | Getting Started with Linux OS Development on SAM9X60 Evaluation Kit | SAM9X60-EK | Getting started with Linux OS development on the SAM9X60-EK board |
| 39 | eXecute-In-Place (XIP) with Serial Flash Memories on MPUs Using MPLAB Harmony V3 (AN5218) | SAM9X60-EK | Application note describing how to execute a Harmony application from an on-board QSPI Flash memory |
| 40 | QSPI-XIP- Example | SAM9X60-EK | Harmony application getting executed from QSPI flash on the SAM9X60 evaluation kit |
| 41 | Attaching the TM5000 WVGA Display | SAM9X60-EK | How to attach the TM5000 WVGA display with SAM9X60-EK |