5 SAMA5D2 Series
| No. | Title/Link |
Hardware Board/ Kit Used | Description |
|---|---|---|---|
| 1 | Developing Applications with MPLAB Harmony v3 Software Framework for MPUs | N/A | Step-by-step guide explaining:
|
| 2 | SAMA5D2 Series Boot Process Training Module | SAMA5D2 Series | Boot process of the SAMA5D2 series microprocessors (MPUs) |
| 3 | MPLAB Discover Code Examples | SAMA5D2 Series | MPLAB Discover code examples |
| 4 | MPLAB github Examples | SAMA5D2 Series | MPLAB Harmony v3 application examples (CSP, Graphics, Ethernet, etc.) |
| 5 | ATSAMA5D27-SOM1-EK1 Evaluation Kit Introduction | ATSAMA5D27 SOM1-EK | Introduction to the SAMA5D27 SOM1-EK board |
| 6 | ATSAMA5D27-SOM1-EK1 Evaluation Kit - Features | ATSAMA5D27 SOM1-EK | Features of the SAMA5D27-SOM1-EK1 board (ATSAMA5D27-SOM1-EK1) |
| 7 | ATSAMA5D27-SOM1-EK1 - Booting a Demo Linux Image from SD Card | ATSAMA5D27 SOM1-EK | Step-by-step instructions detailing how to boot a demo Linux image from an SD card |
| 8 | ATSAMA5D27-SOM1-EK1 - Booting a Linux Image from QSPI Flash Memory | ATSAMA5D27 SOM1-EK | How to configure and program the second- and third-stage bootloaders at91bootstrap and u-boot-at91 from a NOR Flash (QSPI) memory |
| 9 | Starting Linux OS Development on SAMA5D27 SOM1 Evaluation Kit | SAMA5D27 SOM1-EK | Step-by-step guide explaining how to get started developing a Linux OS application on the SAMA5D27-SOM1-EK |
| 10 | Starting Linux OS Development on SAMA5D27 WLSOM1 Evaluation Kit | SAMA5D27 WLSOM1-EK | Step-by-step guide explaining how to get started developing a Linux OS application on the SAMA5D27-WLSOM1-EK |
| 11 | Starting Linux OS Development on SAMA5D2-ICP Board | SAMA5D2-ICP board | Step-by-step guide explaining how to get started developing a Linux OS application on the SAMA5D2-ICP board |
| 12 | Download Buildroot to Create Binary Image Files to Flash onto an SD Memory Card for ATSAMA5D27 SOM1 EK1 Evaluation Kit | ATSAMA5D27-SOM1-EK1 | Step-by-step instructions explaining how to download Buildroot and create binary image files ready to Flash onto an SD memory card using a default or custom configuration for the target: ATSAMA5D27 SOM1 EK1 Evaluation Kit |
| 13 | Develop the following embedded Linux applications using Buildroot: | ATSAMA5D27-SOM1-EK1 | A step-by-step guide on how to develop the following embedded Linux applications using Buildroot: |
| Pin Control and GPIO | Pin Control and GPIO | ||
| ADC | ADC | ||
| Real-time Clock (RTC) | Real-time Clock (RTC) | ||
| I²C | I²C | ||
| SPI | SPI | ||
| Watchdog Timer | Watchdog Timer (WDT) | ||
| Pulse Width Modulation (PWM) | Pulse Width Modulation (PWM) | ||
| UART | UART | ||
| GPIO Based IRQ | GPIO Based IRQ | ||
| USB Mass Storage | USB Mass Storage | ||
| Console UART | Console UART | ||
| 14 | ATSAMA5D27-SOM1-EK1 - Booting a Demo Linux Image from an SD Card | ATSAMA5D27-SOM1-EK1 | How to flash a demo Linux image to an SD card with Etcher |
| 15 | Measuring Power and Energy Consumption Using PAC1934 Monitor with Linux | SAMA5D27-SOM1-EK1 | How to measure power and energy consumption using the PAC1934 monitor with Linux |
| 16 | SAM-BA In-System Programmer (ISP) | N/A | Introduction to SAM-BA ISP and the command line interface |