2 SAMA7G54
| No. | Title/Link |
Hardware Board/ Kit Used | Description |
|---|---|---|---|
| 1 | Developing Applications with MPLAB Harmony v3 Software Framework for MPUs | N/A | Step-by-step guide explaining:
|
| 2 | Booting from External Non-Volatile Memory (NVM) on SAMA7G5 MPUs (AN4408) | SAMA7G5 Series | Application note explaining the boot process of the SAMA7G5 series microprocessors (MPU) |
| 3 | MPLAB Discover Code Examples | SAMA7G5 series | MPLAB Discover code examples |
| 4 | MPLAB github Examples | SAMA7G5 series | MPLAB Harmony v3 application examples (CSP, Graphics, Ethernet, etc.) |
| 5 | SAMA7G54-EK Evaluation Kit Introduction | SAMA7G54-EK | Introduction to the SAMA7G54 Evaluation Kit |
| 6 | SAMA7G54-EK Features | SAMA7G54-EK | SAMA7G54-EK features |
| 7 | QSPI-XIP Example | SAMA7G54-EK | How to execute an MPLAB Harmony application from QSPI flash on SAMA7G54 Evaluation Kit |
| 8 | SAMA7G54-EK | How to connect a host computer running a terminal emulation program to the SAMA7G54-EK serial debug port to access the console | |
| 9 | SAM MPU's: Procedure to build at91bootstrap to boot Harmony application from QSPI in SAMA7G54-EK using MPLAB X IDE | SAMA7G54-EK | How to configure and build the second stage bootloader to boot an MPLAB Harmony application from QSPI (Octa SPI) |
| 10 | Booting Demo Linux Image | SAMA7G54-EK | How to boot a demo Linux image on an SD card and e.MMC |
| 11 | SAM MPU’s: Procedure to Load Boot Configuration Packet to OTPC or Emulation SRAM in SAMA7G54-EK | SAMA7G54-EK | How to configure Boot Configuration Packet (BCP) to boot at91bootstrap from QSPI Flash using SAM-BA by writing BCP to OTPC or Emulation SRAM |
| 12 | Configure and Build at91bootstrap for an MPLAB Harmony v3 Project with MPLAB X IDE | SAMA7G54-EK | How to configure and build at91bootstrap for an MPLAB Harmony v3 project with MPLAB X IDE |
| 13 | Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from e.MMC Flash Memory | SAMA7G54-EK | How to configure and build at91bootstrap to load an MPLAB Harmony v3 application from an e.MMC Flash memory |
| 14 | Writing MPLAB Harmony v3 Application and at91bootstrap to e.MMC Flash Memory using SAM-BA® ISP | SAMA7G54-EK | How to write MPLAB Harmony v3 application and at91bootstrap to an e.MMC Flash memory using SAM-BA In-System Programmer (ISP) |
| 15 | Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from NOR Flash (QSPI) Memory | SAMA7G54-EK | How to configure and build at91bootstrap to load an MPLAB Harmony v3 application from a QSPI NOR Flash memory |
| 16 | Writing MPLAB Harmony v3 Application and at91bootstrap to NOR Flash (QSPI) Memory using SAM-BA ISP | SAMA7G54-EK | How to write an MPLAB Harmony v3 application and at91bootstrap to a QSPI NOR Flash memory using SAM-BA ISP |
| 17 | Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from SD Memory Card | SAMA7G54-EK | How to configure and build at91bootstrap to load an MPLAB Harmony v3 application from an SD card Flash memory |
| 18 | Copy MPLAB Harmony v3 Application and at91bootstrap to SD Memory Card | SAMA7G54-EK | How to write an MPLAB Harmony v3 application and at91bootstrap to an SD card |
| 19 | Getting Started with MPLAB Harmony v3 Development: CSP Application: pio_led_on_off_interrupt | SAMA7G54-EK | How to get started on a CSP Harmony application with SAMA7G54-EK board on MPLAB X IDE |
| 20 | eXecute-In-Place (XIP) with Serial Flash Memories on MPUs Using MPLAB Harmony V3 (AN5218) | SAMA7G54-EK | Application note describing how to execute a Harmony application from QSPI Flash on board |
| 21 | Getting Started on Linux OS Development | SAMA7G54-EK | Getting started on Linux OS development |
| 22 | Booting Linux on SAMA7G5 Series MPU from e.MMC (TB3352) | SAMA7G54-EK | How to boot a Linux image from e.MMC |
| 23 | SAM-BA In-System Programmer (ISP) | N/A | SAM-BA ISP and command line interface |