11.4 Enabling a Peripheral
In order to enable a peripheral that is clocked by a generic clock, the following parts of the system needs to be configured:
- A running clock source.
- A clock from the generic clock generator must be configured to use one of the running clock sources, and the generator must be enabled.
- The generic clock multiplexer that provides the generic clock signal to the peripheral must be configured to use a running generic clock generator, and the generic clock must be enabled.
- The user interface of the peripheral
needs to be unmasked in the PM. If this is not done the peripheral registers will read
all ‘
0’s and any writing attempts to the peripheral will be discarded.