2.3.2 The PGA Initialization Delay Does Not Work Outside Low Latency Mode
0’. This may cause a corrupt conversion when the PGA is the module with the slowest initialization time. When using the internal references, this is not an issue because of a slower initialization delay.Work Around
Set the ADC in low latency mode by setting the Low Latency (LOWLAT) bit in the Control A (CTRLA) register to ‘1’.
Affected Silicon Revisions
| Rev. A |
| X |