9 Document Revision History
| Revision | Date | Section | Description |
|---|---|---|---|
| J | 09/2023 | Introduction | Updated the Linux Kernel path for version 6.1 |
| Cloning a Kernel Source and Root File System | Updated Github tags for Linux Kernel 6.1 and repositories to linux4microchip | ||
| Buildroot File System and Linux Kernel | Updated uboot revision to v4.0.5 | ||
| H | 09/2022 | Introduction | Updated the Linux Kernel path for version 5.15 |
| Cloning a Kernel Source and Root File System | Updated Github tags for Linux Kernel 5.15 | ||
| Buildroot File System and Linux Kernel | Updated uboot revision to v4.0.3 | ||
| Updating Binary and System Image into the Target Board | Updated | ||
| G | 02/2022 | Introduction | Updated the Linux Kernel path for version 5.10 |
| Buildroot File System and Linux Kernel | Updated | ||
| Building Linux Kernel Individually | Updated Github path for linux4microchip | ||
| Running in the ATWILC Station Mode | Updated STA connection examples with WPA3 Security, Removed the deprecated WEP feature examples | ||
| Running in the ATWILC AP Mode | Updated AP examples with WPA3 Security, Removed the deprecated WEP feature examples | ||
| F | 11/2021 | Introduction | Updated the Linux Kernel path for version 5.10 |
| Building Kernel Image | Updated the build steps for compiling the Linux Kernel version 5.10 | ||
| Initializing the WILC Device | Updated | ||
| Adding WILC Driver Support to Kernel | Updated the steps to configure WILC driver module from the GUI selection window | ||
| SD Express Board | Updated (Mainline driver instead of staging driver) | ||
| Serial Peripheral Interface Board | Updated (Mainline driver instead of staging driver) | ||
| BLE Peripheral Mode Example for BlueZ 5.29 and Later | Updated | ||
| Running in the ATWILC Station Mode | Updated | ||
| Running in the ATWILC AP Mode | Updated | ||
| Running in the ATWILC Concurrent Mode | Updated | ||
| E | 10/2020 | Updating Binary and System Image into the Target Board | Updated the steps to build wilc from Linux4SAM |
| Load SAMA5D4 Configuration File | Updated | ||
| buildroot-at91 output images Files | Updated | ||
| How to Build Linux for SAMA5D4 Xplained | Updated | ||
| Cloning a Kernel Source and Root File System | Updated | ||
| Building and Flashing the System Image into the SAMA5D2 Xplained Ultra Board | Updated | ||
| Build Binaries form Source Code | Updated | ||
| Host Suspend/Resume Mechanism | Updated | ||
| Building the Linux Kernel Individually | Updated | ||
| D | 06/2020 | Building and Flashing the System Image into the SAMA5D2 Xplained Ultra Board | Updated |
| How to Build Linux for SAMA5D4 Xplained | Updated | ||
| Updating Binary and System Image into the Target Board. | Updated | ||
| Building and Flashing the System Image into the SAMA5D3 Xplained Board | Updated | ||
| Building and Flashing the System Image into the SAMA5D27-SOM1-EK1 | Updated | ||
| Prerequisites | Updated | ||
|
| ||
| C | 02/2019 |
|
|
| B | 06/2018 | Document |
|
| A | 08/2017 | Document | Initial Release |
Updated with the new terminologies. For more details, see the following note.
Note: Microchip
is aware that some terminologies used in the technical documents and existing software codes of
this product are outdated and unsuitable. This document may use these new terminologies, which
may or may not reflect on the source codes, software GUIs, and the documents referenced within
this document. The following table shows the relevant terminology changes made in this
document.
| Old Terminology | New Terminology | Description |
|---|---|---|
| Master | Host | The following sections are updated with new terminologies:
|